Hi....
i'm interfacing the 4 switches to tm4c123gh6pz controller using GPIO pins..4 switch for Enter,Back,up,down..
if i'l press the enter key then i can set the value using the Back,up,down key..for example initially i'm display the default value as 1000 Hz..so i suppose to to increment the value from 1000 to 6666..after setting this value i need come back to used mode by pressing the enter key..my doubt is how to comeback to user mode after setting the value???i known this is not the rite way to ask this question here..but i need some one help..
i have attache my code..please help me..Thanks in advance