Hi,
I want to design a PCB using RM46L852ZWT (BGA 0.8mm pitch).
- RM46L852 16- and 32-Bit RISC Flash Microcontroller datasheet (p181) indicates 0.45/0.55mm ball size.
- According to In "General hardware design/BGA PCB design" (http://processors.wiki.ti.com/index.php/General_hardware_design/BGA_PCB_design), for a nominal ball diameter of 0.55, nominal land diameter should be 0.4mm.
- I have downloaded dedicated footprint (RM46Lx ZWT BSDL Model --> spnm026.zip) on TI page (http://www.ti.com/product/RM46L852/toolssoftware), and land diameter is 0.55mm.
- With 0.55mm land, it is not possible to route vias between balls for a class 6 PCB so I should use µVias.
--> What would be the minimum land size diameter for the footprint of the RM46L852ZWT BGA ? 0.55mm seems to big ! Could it be 0.4mm, that would make easier the placement of fan out vias ?
Thank you.