Hi,
Trying to find the differences between these two boards. Is there a comparison somewhere? I dont need LED but need CAN & uart support.
Probably going to use TI RTOS but may use freeRTOS.
Advise, links, etc solicited
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jack,
If you are referring to the Tiva Connected Launchpad and Tiva Development kit, I suggest you to get the Tiva Connected launchpad. It is cheaper compared to the Tiva Development kit, and has ethernet connectivity, plus you can connect it to breadboard.
But, if the Tiva Development kit suits you well, and you can afford it, then choose that. I think there is already a CAN port at that board. Check at the User's Guide to be sure.
- kel