Hi,
I wanted to post a modified version of the udma_demo.c for the whoever might need it. I'm new to DMA and thought modifying this example was a good start.
I do have one question. Why am I unable to utilize the internal loopback for the SSI0 interface ?
//*****************************************************************************
//
// udma_demo.c - uDMA example.
//
// Copyright (c) 2013-2014 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
//
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
//
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
//
// This is part of revision 2.1.0.12573 of the EK-TM4C1294XL Firmware Package.
//
//*****************************************************************************
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_uart.h"
#include "inc/hw_ssi.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/uart.h"
#include "driverlib/udma.h"
#include "driverlib/ssi.h"
#include "utils/cpu_usage.h"
#include "utils/uartstdio.h"
#include "utils/ustdlib.h"
//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>uDMA (udma_demo)</h1>
//!
//! This example application demonstrates the use of the uDMA controller to
//! transfer data between memory buffers, and to transfer data to and from a
//! UART. The test runs for 10 seconds before exiting.
//!
//! UART0, connected to the ICDI virtual COM port and running at 115,200,
//! 8-N-1, is used to display messages from this application.
//
//*****************************************************************************
//****************************************************************************
//
// System clock rate in Hz.
//
//****************************************************************************
uint32_t g_ui32SysClock;
//*****************************************************************************
//
// The number of SysTick ticks per second used for the SysTick interrupt.
//
//*****************************************************************************
#define SYSTICKS_PER_SECOND 100
//*****************************************************************************
//
// The size of the memory transfer source and destination buffers (in words).
//
//*****************************************************************************
#define SSI_BUFFER_SIZE 1024
//*****************************************************************************
//
// The size of the UART transmit and receive buffers. They do not need to be
// the same size.
//
//*****************************************************************************
#define UART_TXBUF_SIZE 256
#define UART_RXBUF_SIZE 256
//*****************************************************************************
//
// The SSI0 Buffers
//
//*****************************************************************************
static uint8_t g_ui8SSITxBuf[SSI_BUFFER_SIZE];
static uint8_t g_ui8SSIRxBuf[SSI_BUFFER_SIZE];
//*****************************************************************************
//
// The transmit and receive buffers used for the UART transfers. There is one
// transmit buffer and a pair of recieve ping-pong buffers.
//
//*****************************************************************************
static uint8_t g_ui8TxBuf[UART_TXBUF_SIZE];
static uint8_t g_ui8RxBufA[UART_RXBUF_SIZE];
static uint8_t g_ui8RxBufB[UART_RXBUF_SIZE];
//*****************************************************************************
//
// The count of uDMA errors. This value is incremented by the uDMA error
// handler.
//
//*****************************************************************************
static uint32_t g_ui32uDMAErrCount = 0;
//*****************************************************************************
//
// The count of UART buffers filled, one for each ping-pong buffer.
//
//*****************************************************************************
static uint32_t g_ui32RxBufACount = 0;
static uint32_t g_ui32RxBufBCount = 0;
//*****************************************************************************
//
// The count of SSI0 buffers filled
//
//*****************************************************************************
static uint32_t g_ui32SSIRxCount = 0;
static uint32_t g_ui32SSITxCount = 0;
//*****************************************************************************
//
// The CPU usage in percent, in 16.16 fixed point format.
//
//*****************************************************************************
static uint32_t g_ui32CPUUsage;
//*****************************************************************************
//
// The number of seconds elapsed since the start of the program. This value is
// maintained by the SysTick interrupt handler.
//
//*****************************************************************************
static uint32_t g_ui32Seconds = 0;
//*****************************************************************************
//
// The control table used by the uDMA controller. This table must be aligned
// to a 1024 byte boundary.
//
//*****************************************************************************
#if defined(ewarm)
#pragma data_alignment=1024
uint8_t pui8ControlTable[1024];
#elif defined(ccs)
#pragma DATA_ALIGN(pui8ControlTable, 1024)
uint8_t pui8ControlTable[1024];
#else
uint8_t pui8ControlTable[1024] __attribute__ ((aligned(1024)));
#endif
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
//*****************************************************************************
//
// The interrupt handler for the SysTick timer. This handler will increment a
// seconds counter whenever the appropriate number of ticks has occurred. It
// will also call the CPU usage tick function to find the CPU usage percent.
//
//*****************************************************************************
void
SysTickHandler(void)
{
static uint32_t ui32TickCount = 0;
//
// Increment the tick counter.
//
ui32TickCount++;
//
// If the number of ticks per second has occurred, then increment the
// seconds counter.
//
if(!(ui32TickCount % SYSTICKS_PER_SECOND))
{
g_ui32Seconds++;
}
//
// Call the CPU usage tick function. This function will compute the amount
// of cycles used by the CPU since the last call and return the result in
// percent in fixed point 16.16 format.
//
g_ui32CPUUsage = CPUUsageTick();
}
//*****************************************************************************
//
// The interrupt handler for uDMA errors. This interrupt will occur if the
// uDMA encounters a bus error while trying to perform a transfer. This
// handler just increments a counter if an error occurs.
//
//*****************************************************************************
void
uDMAErrorHandler(void)
{
uint32_t ui32Status;
//
// Check for uDMA error bit
//
ui32Status = ROM_uDMAErrorStatusGet();
//
// If there is a uDMA error, then clear the error and increment
// the error counter.
//
if(ui32Status)
{
ROM_uDMAErrorStatusClear();
g_ui32uDMAErrCount++;
}
}
//*****************************************************************************
//
// SSI0 Interrupt Handler
//
//*****************************************************************************
void
SSI0IntHandler(void)
{
uint32_t ui32Status;
uint32_t ui32Mode;
ui32Status = ROM_SSIIntStatus(SSI0_BASE, 1);
ROM_SSIIntClear(SSI0_BASE, ui32Status);
ui32Mode = ROM_uDMAChannelModeGet(UDMA_CHANNEL_SSI0RX | UDMA_PRI_SELECT);
if(ui32Mode == UDMA_MODE_STOP)
{
g_ui32SSIRxCount++;
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_SSI0RX | UDMA_PRI_SELECT,
UDMA_MODE_BASIC,
(void *)(SSI0_BASE + SSI_O_DR),
g_ui8SSIRxBuf, sizeof(g_ui8SSIRxBuf));
ROM_uDMAChannelEnable(UDMA_CHANNEL_SSI0RX);
}
if(!ROM_uDMAChannelIsEnabled(UDMA_CHANNEL_SSI0TX))
{
g_ui32SSITxCount++;
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_SSI0TX | UDMA_PRI_SELECT,
UDMA_MODE_BASIC, g_ui8SSITxBuf,
(void *)(SSI0_BASE + SSI_O_DR),
sizeof(g_ui8SSITxBuf));
ROM_uDMAChannelEnable(UDMA_CHANNEL_SSI0TX);
}
}
void
InitSPITransfer(void)
{
uint_fast16_t ui16Idx;
//
// Fill the TX buffer with a simple data pattern.
//
for(ui16Idx = 0; ui16Idx < SSI_BUFFER_SIZE; ui16Idx++)
{
g_ui8SSITxBuf[ui16Idx] = ui16Idx;
}
//
// Enable the uDMA interface for both TX and RX channels.
//
ROM_SSIDMAEnable(SSI0_BASE, SSI_DMA_RX | SSI_DMA_TX);
//
// This register write will set the SSI0 to operate in loopback mode. Any
// data sent on the TX output will be received on the RX input.
//
//HWREG(SSI1_BASE + SSI_O_CR1) |= SSI_CR1_LBM;
//****************************************************************************
//uDMA SSI0 RX
//****************************************************************************
//
// Put the attributes in a known state for the uDMA SSI0RX channel. These
// should already be disabled by default.
//
ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_SSI0RX,
UDMA_ATTR_USEBURST | UDMA_ATTR_ALTSELECT |
(UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK));
//
// Configure the control parameters for the primary control structure for
// the SSIORX channel.
//
ROM_uDMAChannelControlSet(UDMA_CHANNEL_SSI0RX | UDMA_PRI_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
UDMA_ARB_4);
//
// Set up the transfer parameters for the SSI0RX Channel
//
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_SSI0RX | UDMA_PRI_SELECT,
UDMA_MODE_BASIC,
(void *)(SSI0_BASE + SSI_O_DR),
g_ui8SSIRxBuf, sizeof(g_ui8SSIRxBuf));
//****************************************************************************
//uDMA SSI0 TX
//****************************************************************************
//
// Put the attributes in a known state for the uDMA SSI0TX channel. These
// should already be disabled by default.
//
ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_SSI0TX,
UDMA_ATTR_ALTSELECT |
UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK);
//
// Set the USEBURST attribute for the uDMA SSI0TX channel. This will
// force the controller to always use a burst when transferring data from
// the TX buffer to the SSI0. This is somewhat more effecient bus usage
// than the default which allows single or burst transfers.
//
ROM_uDMAChannelAttributeEnable(UDMA_CHANNEL_SSI0TX, UDMA_ATTR_USEBURST);
//
// Configure the control parameters for the SSI0 TX.
//
ROM_uDMAChannelControlSet(UDMA_CHANNEL_SSI0TX | UDMA_PRI_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_8 | UDMA_DST_INC_NONE |
UDMA_ARB_4);
//
// Set up the transfer parameters for the uDMA SSI0 TX channel. This will
// configure the transfer source and destination and the transfer size.
// Basic mode is used because the peripheral is making the uDMA transfer
// request. The source is the TX buffer and the destination is theUART0
// data register.
//
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_SSI0TX | UDMA_PRI_SELECT,
UDMA_MODE_BASIC, g_ui8SSITxBuf,
(void *)(SSI0_BASE + SSI_O_DR),
sizeof(g_ui8SSITxBuf));
//
// Now both the uDMA SSI0 TX and RX channels are primed to start a
// transfer. As soon as the channels are enabled, the peripheral will
// issue a transfer request and the data transfers will begin.
//
ROM_uDMAChannelEnable(UDMA_CHANNEL_SSI0RX);
ROM_uDMAChannelEnable(UDMA_CHANNEL_SSI0TX);
//
// Enable the SSI0 DMA TX/RX interrupts.
//
ROM_SSIIntEnable(SSI0_BASE, SSI_DMATX | SSI_DMARX);
//
// Enable the SSI0 peripheral interrupts.
//
ROM_IntEnable(INT_SSI0);
}
void
ConfigureSSI0(void)
{
uint32_t trashBin[1] = {0};
//
// Enable the SSI0 Peripheral.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);
ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_SSI0);
//
// Configure GPIOA_3 as the SSI Chip Select
//
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTA_BASE, GPIO_PIN_3);
ROM_GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, GPIO_PIN_3);
//
// Configure GPIO Pins for SSI0 mode.
//
ROM_GPIOPinConfigure(GPIO_PA2_SSI0CLK);
ROM_GPIOPinConfigure(GPIO_PA4_SSI0XDAT0);
ROM_GPIOPinConfigure(GPIO_PA5_SSI0XDAT1);
ROM_GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_5 | GPIO_PIN_4 | GPIO_PIN_2);
SSIConfigSetExpClk(SSI0_BASE, g_ui32SysClock, SSI_FRF_MOTO_MODE_3,
SSI_MODE_MASTER, 1000000, 8);
SSIEnable(SSI0_BASE);
/* Clear SSI0 RX Buffer */
while (ROM_SSIDataGetNonBlocking(SSI0_BASE, &trashBin[0])) {}
}
//*****************************************************************************
//
// The interrupt handler for UART1. This interrupt will occur when a DMA
// transfer is complete using the UART1 uDMA channel. It will also be
// triggered if the peripheral signals an error. This interrupt handler will
// switch between receive ping-pong buffers A and B. It will also restart a TX
// uDMA transfer if the prior transfer is complete. This will keep the UART
// running continuously (looping TX data back to RX).
//
//*****************************************************************************
void
UART1IntHandler(void)
{
uint32_t ui32Status;
uint32_t ui32Mode;
//
// Read the interrupt status of the UART.
//
ui32Status = ROM_UARTIntStatus(UART1_BASE, 1);
//
// Clear any pending status, even though there should be none since no UART
// interrupts were enabled. If UART error interrupts were enabled, then
// those interrupts could occur here and should be handled. Since uDMA is
// used for both the RX and TX, then neither of those interrupts should be
// enabled.
//
ROM_UARTIntClear(UART1_BASE, ui32Status);
//
// Check the DMA control table to see if the ping-pong "A" transfer is
// complete. The "A" transfer uses receive buffer "A", and the primary
// control structure.
//
ui32Mode = ROM_uDMAChannelModeGet(UDMA_CHANNEL_UART1RX | UDMA_PRI_SELECT);
//
// If the primary control structure indicates stop, that means the "A"
// receive buffer is done. The uDMA controller should still be receiving
// data into the "B" buffer.
//
if(ui32Mode == UDMA_MODE_STOP)
{
//
// Increment a counter to indicate data was received into buffer A. In
// a real application this would be used to signal the main thread that
// data was received so the main thread can process the data.
//
g_ui32RxBufACount++;
//
// Set up the next transfer for the "A" buffer, using the primary
// control structure. When the ongoing receive into the "B" buffer is
// done, the uDMA controller will switch back to this one. This
// example re-uses buffer A, but a more sophisticated application could
// use a rotating set of buffers to increase the amount of time that
// the main thread has to process the data in the buffer before it is
// reused.
//
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,
(void *)(UART1_BASE + UART_O_DR),
g_ui8RxBufA, sizeof(g_ui8RxBufA));
}
//
// Check the DMA control table to see if the ping-pong "B" transfer is
// complete. The "B" transfer uses receive buffer "B", and the alternate
// control structure.
//
ui32Mode = ROM_uDMAChannelModeGet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT);
//
// If the alternate control structure indicates stop, that means the "B"
// receive buffer is done. The uDMA controller should still be receiving
// data into the "A" buffer.
//
if(ui32Mode == UDMA_MODE_STOP)
{
//
// Increment a counter to indicate data was received into buffer A. In
// a real application this would be used to signal the main thread that
// data was received so the main thread can process the data.
//
g_ui32RxBufBCount++;
//
// Set up the next transfer for the "B" buffer, using the alternate
// control structure. When the ongoing receive into the "A" buffer is
// done, the uDMA controller will switch back to this one. This
// example re-uses buffer B, but a more sophisticated application could
// use a rotating set of buffers to increase the amount of time that
// the main thread has to process the data in the buffer before it is
// reused.
//
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT,
UDMA_MODE_PINGPONG,
(void *)(UART1_BASE + UART_O_DR),
g_ui8RxBufB, sizeof(g_ui8RxBufB));
}
//
// If the UART1 DMA TX channel is disabled, that means the TX DMA transfer
// is done.
//
if(!ROM_uDMAChannelIsEnabled(UDMA_CHANNEL_UART1TX))
{
//
// Start another DMA transfer to UART1 TX.
//
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1TX | UDMA_PRI_SELECT,
UDMA_MODE_BASIC, g_ui8TxBuf,
(void *)(UART1_BASE + UART_O_DR),
sizeof(g_ui8TxBuf));
//
// The uDMA TX channel must be re-enabled.
//
ROM_uDMAChannelEnable(UDMA_CHANNEL_UART1TX);
}
}
//*****************************************************************************
//
// Initializes the UART1 peripheral and sets up the TX and RX uDMA channels.
// The UART is configured for loopback mode so that any data sent on TX will be
// received on RX. The uDMA channels are configured so that the TX channel
// will copy data from a buffer to the UART TX output. And the uDMA RX channel
// will receive any incoming data into a pair of buffers in ping-pong mode.
//
//*****************************************************************************
void
InitUART1Transfer(void)
{
uint_fast16_t ui16Idx;
//
// Fill the TX buffer with a simple data pattern.
//
for(ui16Idx = 0; ui16Idx < UART_TXBUF_SIZE; ui16Idx++)
{
g_ui8TxBuf[ui16Idx] = ui16Idx;
}
//
// Enable the UART peripheral, and configure it to operate even if the CPU
// is in sleep.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1);
ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UART1);
//
// Configure the UART communication parameters.
//
ROM_UARTConfigSetExpClk(UART1_BASE, g_ui32SysClock, 115200,
UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE);
//
// Set both the TX and RX trigger thresholds to 4. This will be used by
// the uDMA controller to signal when more data should be transferred. The
// uDMA TX and RX channels will be configured so that it can transfer 4
// bytes in a burst when the UART is ready to transfer more data.
//
ROM_UARTFIFOLevelSet(UART1_BASE, UART_FIFO_TX4_8, UART_FIFO_RX4_8);
//
// Enable the UART for operation, and enable the uDMA interface for both TX
// and RX channels.
//
ROM_UARTEnable(UART1_BASE);
ROM_UARTDMAEnable(UART1_BASE, UART_DMA_RX | UART_DMA_TX);
//
// This register write will set the UART to operate in loopback mode. Any
// data sent on the TX output will be received on the RX input.
//
HWREG(UART1_BASE + UART_O_CTL) |= UART_CTL_LBE;
//
// Put the attributes in a known state for the uDMA UART1RX channel. These
// should already be disabled by default.
//
ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_UART1RX,
UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST |
UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK);
//
// Configure the control parameters for the primary control structure for
// the UART RX channel. The primary contol structure is used for the "A"
// part of the ping-pong receive. The transfer data size is 8 bits, the
// source address does not increment since it will be reading from a
// register. The destination address increment is byte 8-bit bytes. The
// arbitration size is set to 4 to match the RX FIFO trigger threshold.
// The uDMA controller will use a 4 byte burst transfer if possible. This
// will be somewhat more effecient that single byte transfers.
//
ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART1RX | UDMA_PRI_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
UDMA_ARB_4);
//
// Configure the control parameters for the alternate control structure for
// the UART RX channel. The alternate contol structure is used for the "B"
// part of the ping-pong receive. The configuration is identical to the
// primary/A control structure.
//
ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
UDMA_ARB_4);
//
// Set up the transfer parameters for the UART RX primary control
// structure. The mode is set to ping-pong, the transfer source is the
// UART data register, and the destination is the receive "A" buffer. The
// transfer size is set to match the size of the buffer.
//
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,
(void *)(UART1_BASE + UART_O_DR),
g_ui8RxBufA, sizeof(g_ui8RxBufA));
//
// Set up the transfer parameters for the UART RX alternate control
// structure. The mode is set to ping-pong, the transfer source is the
// UART data register, and the destination is the receive "B" buffer. The
// transfer size is set to match the size of the buffer.
//
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT,
UDMA_MODE_PINGPONG,
(void *)(UART1_BASE + UART_O_DR),
g_ui8RxBufB, sizeof(g_ui8RxBufB));
//
// Put the attributes in a known state for the uDMA UART1TX channel. These
// should already be disabled by default.
//
ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_UART1TX,
UDMA_ATTR_ALTSELECT |
UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK);
//
// Set the USEBURST attribute for the uDMA UART TX channel. This will
// force the controller to always use a burst when transferring data from
// the TX buffer to the UART. This is somewhat more effecient bus usage
// than the default which allows single or burst transfers.
//
ROM_uDMAChannelAttributeEnable(UDMA_CHANNEL_UART1TX, UDMA_ATTR_USEBURST);
//
// Configure the control parameters for the UART TX. The uDMA UART TX
// channel is used to transfer a block of data from a buffer to the UART.
// The data size is 8 bits. The source address increment is 8-bit bytes
// since the data is coming from a buffer. The destination increment is
// none since the data is to be written to the UART data register. The
// arbitration size is set to 4, which matches the UART TX FIFO trigger
// threshold.
//
ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART1TX | UDMA_PRI_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_8 |
UDMA_DST_INC_NONE |
UDMA_ARB_4);
//
// Set up the transfer parameters for the uDMA UART TX channel. This will
// configure the transfer source and destination and the transfer size.
// Basic mode is used because the peripheral is making the uDMA transfer
// request. The source is the TX buffer and the destination is the UART
// data register.
//
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1TX | UDMA_PRI_SELECT,
UDMA_MODE_BASIC, g_ui8TxBuf,
(void *)(UART1_BASE + UART_O_DR),
sizeof(g_ui8TxBuf));
//
// Now both the uDMA UART TX and RX channels are primed to start a
// transfer. As soon as the channels are enabled, the peripheral will
// issue a transfer request and the data transfers will begin.
//
ROM_uDMAChannelEnable(UDMA_CHANNEL_UART1RX);
ROM_uDMAChannelEnable(UDMA_CHANNEL_UART1TX);
//
// Enable the UART DMA TX/RX interrupts.
//
ROM_UARTIntEnable(UART1_BASE, UART_INT_DMATX | UART_INT_DMARX);
//
// Enable the UART peripheral interrupts.
//
ROM_IntEnable(INT_UART1);
}
//*****************************************************************************
//
// Configure the UART and its pins. This must be called before UARTprintf().
//
//*****************************************************************************
void
ConfigureUART(void)
{
//
// Enable the GPIO Peripheral used by the UART.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//
// Enable UART0
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UART0);
//
// Configure GPIO Pins for UART mode.
//
ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Initialize the UART for console I/O.
//
UARTStdioConfig(0, 115200, g_ui32SysClock);
}
//*****************************************************************************
//
// This example demonstrates how to use the uDMA controller to transfer data
// between memory buffers and to and from a peripheral, in this case a UART.
// The uDMA controller is configured to repeatedly transfer a block of data
// from one memory buffer to another. It is also set up to repeatedly copy a
// block of data from a buffer to the UART output. The UART data is looped
// back so the same data is received, and the uDMA controlled is configured to
// continuously receive the UART data using ping-pong buffers.
//
// The processor is put to sleep when it is not doing anything, and this allows
// collection of CPU usage data to see how much CPU is being used while the
// data transfers are ongoing.
//
//*****************************************************************************
int
main(void)
{
static uint32_t ui32PrevSeconds;
static uint32_t ui32PrevXferCount;
static uint32_t ui32PrevUARTCount = 0;
uint32_t ui32XfersCompleted;
uint32_t ui32BytesTransferred;
//
// Set the clocking to run directly from the crystal at 120MHz.
//
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
//
// Enable peripherals to operate when CPU is in sleep.
//
ROM_SysCtlPeripheralClockGating(true);
//
// Enable the GPIO port that is used for the on-board LED.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
//
// Enable the GPIO port that is used for the SSI chip select
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//
// Enable the GPIO pins for the LED (PN0).
//
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0);
//
// Initialize the UART.
//
ConfigureUART();
UARTprintf("\033[2J\033[H");
UARTprintf("uDMA Example\n");
//
// Initialize SSI0.
//
ConfigureSSI0();
//
// Show the clock frequency on the display.
//
UARTprintf("Tiva C Series @ %u MHz\n\n", g_ui32SysClock / 1000000);
//
// Show statistics headings.
//
UARTprintf("CPU\tRemaining\tSSI TX\t\t\t UART\n");
UARTprintf("Usage\tTime\t\tTransfers\t\t Transfers\n");
//
// Configure SysTick to occur 100 times per second, to use as a time
// reference. Enable SysTick to generate interrupts.
//
ROM_SysTickPeriodSet(g_ui32SysClock / SYSTICKS_PER_SECOND);
ROM_SysTickIntEnable();
ROM_SysTickEnable();
//
// Initialize the CPU usage measurement routine.
//
CPUUsageInit(g_ui32SysClock, SYSTICKS_PER_SECOND, 2);
//
// Enable the uDMA controller at the system level. Enable it to continue
// to run while the processor is in sleep.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UDMA);
//
// Enable the uDMA controller error interrupt. This interrupt will occur
// if there is a bus error during a transfer.
//
ROM_IntEnable(INT_UDMAERR);
//
// Enable the uDMA controller.
//
ROM_uDMAEnable();
//
// Point at the control table to use for channel control structures.
//
ROM_uDMAControlBaseSet(pui8ControlTable);
//
// Initialize the uDMA SPI transfers.
//
InitSPITransfer();
//
// Initialize the uDMA UART transfers.
//
InitUART1Transfer();
//
// Remember the current SysTick seconds count.
//
ui32PrevSeconds = g_ui32Seconds;
//
// Remember the current count of memory buffer transfers.
//
ui32PrevXferCount = g_ui32SSITxCount;
//
// Loop until the button is pressed. The processor is put to sleep
// in this loop so that CPU utilization can be measured.
//
while(1)
{
//
// Check to see if one second has elapsed. If so, the make some
// updates.
//
if(g_ui32Seconds != ui32PrevSeconds)
{
//
// Turn on the LED as a heartbeat
//
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0);
//
// Print a message showing the CPU usage percent.
// The fractional part of the percent value is ignored.
//
UARTprintf("%2u%%", g_ui32CPUUsage >> 16);
//
// Tell the user how many seconds we have to go before ending.
//
UARTprintf("\t%d seconds", 10 - g_ui32Seconds);
//
// Remember the new seconds count.
//
ui32PrevSeconds = g_ui32Seconds;
//
// Calculate how many memory transfers have occurred since the last
// second.
//
ui32XfersCompleted = g_ui32SSITxCount - ui32PrevXferCount;
//
// Remember the new transfer count.
//
ui32PrevXferCount = g_ui32SSITxCount++;;
//
// Compute how many bytes were transferred in the memory transfer
// since the last second.
//
ui32BytesTransferred = ui32XfersCompleted * SSI_BUFFER_SIZE * 4;
//
// Print a message showing the transfer rate.
//
UARTprintf("\t%8u Bytes/Sec", ui32BytesTransferred);
//
// Calculate how many UART transfers have occurred since the last
// second. This expression is split to prevent a compiler warning
// about undefined order of volatile accesses.
//
ui32XfersCompleted = g_ui32RxBufACount;
ui32XfersCompleted += g_ui32RxBufBCount - ui32PrevUARTCount;
//
// Remember the new UART transfer count. This expression is split
// to prevent a compiler warning about undefined order of volatile
// accesses.
//
ui32PrevUARTCount = g_ui32RxBufACount;
ui32PrevUARTCount += g_ui32RxBufBCount;
//
// Compute how many bytes were transferred by the UART. The number
// of bytes received is multiplied by 2 so that the TX bytes
// transferred are also accounted for.
//
ui32BytesTransferred = ui32XfersCompleted * UART_RXBUF_SIZE * 2;
//
// Print a message showing the transfer rate.
//
UARTprintf("\t%8u Bytes/Sec\n", ui32BytesTransferred);
//
// Turn off the LED.
//
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, ~GPIO_PIN_0);
}
//
// Put the processor to sleep if there is nothing to do. This allows
// the CPU usage routine to measure the number of free CPU cycles.
// If the processor is sleeping a lot, it can be hard to connect to
// the target with the debugger.
//
ROM_SysCtlSleep();
//
// See if we have run long enough and exit the loop if so.
//
if(g_ui32Seconds >= 10)
{
break;
}
}
//
// Indicate on the display that the example is stopped.
//
UARTprintf("\nStopped\n");
ROM_IntDisable(INT_UART1);
ROM_IntDisable(INT_SSI0);
//
// Loop forever with the CPU not sleeping, so the debugger can connect.
//
while(1)
{
//
// Turn on the LED.
//
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0);
//
// Delay for a bit.
//
SysCtlDelay(g_ui32SysClock / 20 / 3);
//
// Turn off the LED.
//
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0);
//
// Delay for a bit.
//
SysCtlDelay(g_ui32SysClock / 20 / 3);
}
}
//*****************************************************************************
//
// startup_ccs.c - Startup code for use with TI's Code Composer Studio.
//
// Copyright (c) 2013-2014 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
//
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
//
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
//
// This is part of revision 2.1.0.12573 of the EK-TM4C1294XL Firmware Package.
//
//*****************************************************************************
#include <stdint.h>
#include "inc/hw_nvic.h"
#include "inc/hw_types.h"
//*****************************************************************************
//
// Forward declaration of the default fault handlers.
//
//*****************************************************************************
void ResetISR(void);
static void NmiSR(void);
static void FaultISR(void);
static void IntDefaultHandler(void);
//*****************************************************************************
//
// External declaration for the reset handler that is to be called when the
// processor is started
//
//*****************************************************************************
extern void _c_int00(void);
//*****************************************************************************
//
// Linker variable that marks the top of the stack.
//
//*****************************************************************************
extern uint32_t __STACK_TOP;
//*****************************************************************************
//
// External declarations for the interrupt handlers used by the application.
//
//*****************************************************************************
extern void SysTickHandler(void);
extern void UART1IntHandler(void);
extern void SSI0IntHandler(void);
extern void uDMAErrorHandler(void);
//*****************************************************************************
//
// The vector table. Note that the proper constructs must be placed on this to
// ensure that it ends up at physical address 0x0000.0000 or at the start of
// the program if located at a start address other than 0.
//
//*****************************************************************************
#pragma DATA_SECTION(g_pfnVectors, ".intvecs")
void (* const g_pfnVectors[])(void) =
{
(void (*)(void))((uint32_t)&__STACK_TOP),
// The initial stack pointer
ResetISR, // The reset handler
NmiSR, // The NMI handler
FaultISR, // The hard fault handler
IntDefaultHandler, // The MPU fault handler
IntDefaultHandler, // The bus fault handler
IntDefaultHandler, // The usage fault handler
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
IntDefaultHandler, // SVCall handler
IntDefaultHandler, // Debug monitor handler
0, // Reserved
IntDefaultHandler, // The PendSV handler
SysTickHandler, // The SysTick handler
IntDefaultHandler, // GPIO Port A
IntDefaultHandler, // GPIO Port B
IntDefaultHandler, // GPIO Port C
IntDefaultHandler, // GPIO Port D
IntDefaultHandler, // GPIO Port E
IntDefaultHandler, // UART0 Rx and Tx
UART1IntHandler, // UART1 Rx and Tx
SSI0IntHandler, // SSI0 Rx and Tx
IntDefaultHandler, // I2C0 Master and Slave
IntDefaultHandler, // PWM Fault
IntDefaultHandler, // PWM Generator 0
IntDefaultHandler, // PWM Generator 1
IntDefaultHandler, // PWM Generator 2
IntDefaultHandler, // Quadrature Encoder 0
IntDefaultHandler, // ADC Sequence 0
IntDefaultHandler, // ADC Sequence 1
IntDefaultHandler, // ADC Sequence 2
IntDefaultHandler, // ADC Sequence 3
IntDefaultHandler, // Watchdog timer
IntDefaultHandler, // Timer 0 subtimer A
IntDefaultHandler, // Timer 0 subtimer B
IntDefaultHandler, // Timer 1 subtimer A
IntDefaultHandler, // Timer 1 subtimer B
IntDefaultHandler, // Timer 2 subtimer A
IntDefaultHandler, // Timer 2 subtimer B
IntDefaultHandler, // Analog Comparator 0
IntDefaultHandler, // Analog Comparator 1
IntDefaultHandler, // Analog Comparator 2
IntDefaultHandler, // System Control (PLL, OSC, BO)
IntDefaultHandler, // FLASH Control
IntDefaultHandler, // GPIO Port F
IntDefaultHandler, // GPIO Port G
IntDefaultHandler, // GPIO Port H
IntDefaultHandler, // UART2 Rx and Tx
IntDefaultHandler, // SSI1 Rx and Tx
IntDefaultHandler, // Timer 3 subtimer A
IntDefaultHandler, // Timer 3 subtimer B
IntDefaultHandler, // I2C1 Master and Slave
IntDefaultHandler, // CAN0
IntDefaultHandler, // CAN1
IntDefaultHandler, // Ethernet
IntDefaultHandler, // Hibernate
IntDefaultHandler, // USB0
IntDefaultHandler, // PWM Generator 3
IntDefaultHandler, // uDMA Software Transfer
uDMAErrorHandler, // uDMA Error
IntDefaultHandler, // ADC1 Sequence 0
IntDefaultHandler, // ADC1 Sequence 1
IntDefaultHandler, // ADC1 Sequence 2
IntDefaultHandler, // ADC1 Sequence 3
IntDefaultHandler, // External Bus Interface 0
IntDefaultHandler, // GPIO Port J
IntDefaultHandler, // GPIO Port K
IntDefaultHandler, // GPIO Port L
IntDefaultHandler, // SSI2 Rx and Tx
IntDefaultHandler, // SSI3 Rx and Tx
IntDefaultHandler, // UART3 Rx and Tx
IntDefaultHandler, // UART4 Rx and Tx
IntDefaultHandler, // UART5 Rx and Tx
IntDefaultHandler, // UART6 Rx and Tx
IntDefaultHandler, // UART7 Rx and Tx
IntDefaultHandler, // I2C2 Master and Slave
IntDefaultHandler, // I2C3 Master and Slave
IntDefaultHandler, // Timer 4 subtimer A
IntDefaultHandler, // Timer 4 subtimer B
IntDefaultHandler, // Timer 5 subtimer A
IntDefaultHandler, // Timer 5 subtimer B
IntDefaultHandler, // FPU
0, // Reserved
0, // Reserved
IntDefaultHandler, // I2C4 Master and Slave
IntDefaultHandler, // I2C5 Master and Slave
IntDefaultHandler, // GPIO Port M
IntDefaultHandler, // GPIO Port N
0, // Reserved
IntDefaultHandler, // Tamper
IntDefaultHandler, // GPIO Port P (Summary or P0)
IntDefaultHandler, // GPIO Port P1
IntDefaultHandler, // GPIO Port P2
IntDefaultHandler, // GPIO Port P3
IntDefaultHandler, // GPIO Port P4
IntDefaultHandler, // GPIO Port P5
IntDefaultHandler, // GPIO Port P6
IntDefaultHandler, // GPIO Port P7
IntDefaultHandler, // GPIO Port Q (Summary or Q0)
IntDefaultHandler, // GPIO Port Q1
IntDefaultHandler, // GPIO Port Q2
IntDefaultHandler, // GPIO Port Q3
IntDefaultHandler, // GPIO Port Q4
IntDefaultHandler, // GPIO Port Q5
IntDefaultHandler, // GPIO Port Q6
IntDefaultHandler, // GPIO Port Q7
IntDefaultHandler, // GPIO Port R
IntDefaultHandler, // GPIO Port S
IntDefaultHandler, // SHA/MD5 0
IntDefaultHandler, // AES 0
IntDefaultHandler, // DES3DES 0
IntDefaultHandler, // LCD Controller 0
IntDefaultHandler, // Timer 6 subtimer A
IntDefaultHandler, // Timer 6 subtimer B
IntDefaultHandler, // Timer 7 subtimer A
IntDefaultHandler, // Timer 7 subtimer B
IntDefaultHandler, // I2C6 Master and Slave
IntDefaultHandler, // I2C7 Master and Slave
IntDefaultHandler, // HIM Scan Matrix Keyboard 0
IntDefaultHandler, // One Wire 0
IntDefaultHandler, // HIM PS/2 0
IntDefaultHandler, // HIM LED Sequencer 0
IntDefaultHandler, // HIM Consumer IR 0
IntDefaultHandler, // I2C8 Master and Slave
IntDefaultHandler, // I2C9 Master and Slave
IntDefaultHandler // GPIO Port T
};
//*****************************************************************************
//
// This is the code that gets called when the processor first starts execution
// following a reset event. Only the absolutely necessary set is performed,
// after which the application supplied entry() routine is called. Any fancy
// actions (such as making decisions based on the reset cause register, and
// resetting the bits in that register) are left solely in the hands of the
// application.
//
//*****************************************************************************
void
ResetISR(void)
{
//
// Jump to the CCS C initialization routine. This will enable the
// floating-point unit as well, so that does not need to be done here.
//
__asm(" .global _c_int00\n"
" b.w _c_int00");
}
//*****************************************************************************
//
// This is the code that gets called when the processor receives a NMI. This
// simply enters an infinite loop, preserving the system state for examination
// by a debugger.
//
//*****************************************************************************
static void
NmiSR(void)
{
//
// Enter an infinite loop.
//
while(1)
{
}
}
//*****************************************************************************
//
// This is the code that gets called when the processor receives a fault
// interrupt. This simply enters an infinite loop, preserving the system state
// for examination by a debugger.
//
//*****************************************************************************
static void
FaultISR(void)
{
//
// Enter an infinite loop.
//
while(1)
{
}
}
//*****************************************************************************
//
// This is the code that gets called when the processor receives an unexpected
// interrupt. This simply enters an infinite loop, preserving the system state
// for examination by a debugger.
//
//*****************************************************************************
static void
IntDefaultHandler(void)
{
//
// Go into an infinite loop.
//
while(1)
{
}
}
Regards,
Daniel