This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What are the supply requirements for the TMS570LS microcontrollers?

The TMS570xxxx6 microcontroller has two different supply levels required. These are nominally 3.3V and 1.5V.

  • 3.3V supplies:
    • Min required = 3.0V, Max allowed = 3.6V
    • VCCIO: Supply for the I/Os
    • VCCP: Supply for the flash pump
    • VCCAD: Supply for the on-chip Analog-to-Digital Converter (ADC)
    • ADREFHI: High reference voltage for the ADC
  • 1.5V supply:
    • Min required = 1.35V, Max allowed = 1.65V
    • VCC: Supply for the microcontroller core logic and RAM blocks

The external supply regulators must also monitor these supplies and assert power-on reset to the micro whenever any of the supply goes out of regulation.

The full electrical requirements for these supplies are specified in the TMS570LS datasheet at TMS570LS20216/20206/10216/10206/10116/10106 16/32-Bit RISC Flash Microcontroller page 64.