This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123G UART Flow Control



Hey there,

I noticed in the TM4C123G Datasheet mentions flow control on UART1:

"Modem flow control and status (on UART1)"

Just wondering if I can only use UART1 for RTS/CTS and RX/TX?

There's no way I can use U2RX (PD6) for an RTS, correct?

Thanks!

  • Usually (but possibly - not always) there is one, "modem style, UART instantiation" per this class MCU.  Appears that you've read/reviewed the MCU manual - you should encounter a pin-out listing keyed by functionality - (such as ADC, PWM, UART) and this should confirm the presence/absence of any/all "modem style, UART Ports.

    I'm placing a tall chip-stack on, "just one."

    You may "bit-bang" (to functionally extend the normal "abbreviated" UART) - but the built-in capability is so much quicker/easier...

  • Thanks for the reply, the Pin Configurations definitely shows UART1 as the one with CTS / RTS. Looks like I'll have to mess with software interrupts.