This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

need of two microcontrollers in launchpad, Loading program to flash using usb to serial converter

Other Parts Discussed in Thread: ENERGIA

hi,

  I am new to tiva c series family. I am using tm4c123gx launchpad 

1)  i see two micro controllers are used in the board. What is the function of second micro controller.

2)  i am planning to design a circuit using tm4c129x microcontroller. I am using energia ide can i use a usb to  serial converter to load the program to the microcontroller using a usb cable.

3)  As i am new to this microcontroller can u suggest some guidelines to design the circuit

  • ciril Emmanuel james said:
    1)  i see two micro controllers are used in the board. What is the function of second micro controller.

    The other Tiva microcontroller functions as a ICDI. You will understand better if you see the schematic diagram at the User's Guide.

    ciril Emmanuel james said:
    2)  i am planning to design a circuit using tm4c129x microcontroller. I am using energia ide can i use a usb to  serial converter to load the program to the microcontroller using a usb cable.

    Then use a TM4C129 based kit as reference for your design. There is the Tiva Connected Launchpad and the Tiva Development kit. There is already ICDI interface at the board to load your program.

    ciril Emmanuel james said:
    3)  As i am new to this microcontroller can u suggest some guidelines to design the circuit

    Learn some basic electronics and circuits. Maybe you can learn from existing designs.

    - kel

  • Hi ciril,

    I also sugest you visit Stelarisiti.com forum since there's a part for Energia there. In 43oh.com you also can post about Tiva in the Energia section.

    About learning electronics i used google alot, but realy alot. As Markel said, learn from existing projects. I need to limit current? Well search, i didn't understand why there was a transistor with a mosfet and why it was diferent? well search that. Then of course there are forums to help you with what you can't realy understand alone but personaly i don't use E2E for that, i use more those 2 forums i sugested