Hello -
I have a TM4C123GH6PZ unit on a custom board. I'm suddenly unable to program it.
It worked fine for few months, until today.
CORTEX_M4_1: Flash Programmer: Erasing flash contents timed out!
CORTEX_M4_1: Flash Programmer: Timed out while writing to Flash memory
CORTEX_M4_1: GEL: File: C:\work_cc6\XXX_ARM_M4_CCS\Debug\XXX_Arm_M4_CCS.out: Load failed.
CORTEX_M4_1: Unable to terminate memory download: NULL buffer pointer at 0x3a9
Some notes:
1. I tried to program a unit on a different (but same configuration) board, and it worked fine.
2. I tried to do the "Debug Port Unlock" procedure. It seemed to work fine but didn't solve the problem.
3. I'm able to connect to the target using JTAG.
Technical info:
Unit used: TM4C123GH6PZ
XTAL freq: 20MHz, Sysclk freq: 40Mhz
Dev Tool: CCS 6.0.0.00156
JTAG Emulator: XDS100V2
JTAG Freq: 1Mhz
Any possible solution ?
Thanks,
Tal