Hello,
We have prototyped a new board with a TMS570LS3137. Unfortunately the PLL VCC pin was connected to the wrong supply rail. The hardware guys have managed to disconnect the pin but have been unable to connect to the correct voltage. Before they re-spin the board they want to be sure there are no other problems.
The TMS570 has various clock sources. Can the processor run with the PLL VCC pin disconnected?
I tried to connect with a XDS510 USB JTAG interface. The board responds correctly to the test connection script but I can't make it connect. Is it possible to debug using the crystal or one of the internal oscillators only? If so, is there a setting I need to change in the debug configuration?
Thanks,
Richard