Hello,
I have develop a board base on Tiva micro controller TM4C123GH6PZI. I would like to download firmware to microcontroller via UART0 and using the LM flash programmer. The connection between the PC and the micro controller UART0 is done via FTDI USB to RS-232 converter. According to my knowledge the chip shipped with serial flash loader programmer.
I define in the LM flash programmer the following definition
<< OLE Object: Picture (Device Independent Bitmap) >>
<< OLE Object: Picture (Device Independent Bitmap) >>
After pressing the Program button I receive the following message
<< OLE Object: Picture (Device Independent Bitmap) >>
Who can work with me in order to resolve this issue?
Thanks, Shmuel