This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1233H6PM:- THERMAL PRINTER APPLICATION

Other Parts Discussed in Thread: TM4C1233H6PM, UNIFLASH

Hello ,

I am try to build Thermal Printer using TM4C1233H6PM controller with TI's application note and firmware.

The Thermal Head used in my schematics is LTP02-245 from Sekio 

I have assembled the board and powered up and connected with usb . Then , in system it is showing "Stellaries Firmware Upgrade" and I programmed with the firmware given in application note named "THERMAL PRINTER 4F PORTED_V6.out" with uniflash 3.1.0 utility.And shows successfully programmed.

But after programming ,the controller is not at all detecting through usb . And  I don't have any jtag programmers with me for checking . Secondly the flashed program also not working ,I tried with application program "TIVA-

THERMAL PRINTER DEMO INTERFACE"  .in that it is not detecting with serial port .

Please help me for solving the issue.

Schematics attached for reference.

Thermal_Printer.pdf