Other Parts Discussed in Thread: TUSB1105, HALCOGEN, RM46L852
Dear Sirs,
I try to implement the Device USB software. The RM46 is connected to a 6-wire Transceiver TUSB1105 as described in the RM46 Manual SPNU514A (09.14) page 1844. I have check the CLK (VCLKA3_S) 48MHz and IOMM signal multiplexing. After connecting the RM46 changes to attached state and default state. A reset is made by the host and the Reset State is entered.
My PC tries to configure the device but, as I see it will never change in address State. I have also checked the USB registers but I can not see any change. (USB Reset will disable all Interrupts instead of Process Change Interrupt, so at the end of the interrupt routine it will be an interrupt enable)
It is written that the address state will be done automatically.
Under which condition will this fail ?
Are there any register, which must be set within the reset state routine, so that the crossing to the address state will work ?
Best regards A.Friebel