Hi,
I have created a project for RM46 using Halcogen for GCC toolchain, I found after executing code generation command linker file is blank .
or I am doing something wrong?
Please help,
Thanks and regards,
Neha.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have created a project for RM46 using Halcogen for GCC toolchain, I found after executing code generation command linker file is blank .
or I am doing something wrong?
Please help,
Thanks and regards,
Neha.
Hi,
Please find the attached project file in Halcogen.
may i get linker file for GCC?
thanks.
Hi Neha,
It was intentionally left blank, because the GCC port in HALCoGen is done compatible for Atollic Truestudio. As of now Atollic has support only for RM48x and TMS570LS31x family. RM46x debug support is not available even though it is similar to RM48x. We have intimated Atollic to add support for all hercules devices so by next HALCoGen release we will add this support.
With a simple file addition we can generate the linker file for RM46x , TMS570LS12x and TMS570LS11x family of device.
http://e2e.ti.com/cfs-file.ashx/__key/communityserver-discussions-components-files/312/8308.sys_5F00_link.ld
Can you please place the attached sys_link.ld file in the below folder and recreate the project.
C:\ti\Hercules\HALCoGen\v04.01.00\drivers\TMS570LS1227ZWT\SYSTEM570v000