Hello,
I´m using the launchPad tiva and I´m have problems. In my case I need read two channel of the ADC and I get to read when two channel are connected in potentiometers, for example, but when one of the ports (I´m using PE1 and PE2) is floating, there are pulses that are generate in frequency of 1 Hz and my measure is distorted.
Attached the following image when the PE1 is floating and PE2 is connected in potentiometer.
What´s happened?