Other Parts Discussed in Thread: TM4C129ENCPDT
Dear All,
I am developing a product for RS232/RS485 to Ethernet protocol converter using TIVA TM4C129ENCPDT.
Our board will acquire data from smart meter using RS485 and sending the data to another board which will be also having the same controller.
Second device will process the data and will send the data to IEC-101 master.
We have tested the board with serial communication between both the boards.
Now we want to setup Ethernet communication between both the TIVA controller, as both the devices will be residing at different places and will be using GPRS or broadband modem to communicate.
I need to know if there is any sample code to use to setup a communication between both the devices.
I have refered the sample code enet_lwip , enet_IO, enet_Uip but all these codes are used as server.
If I can get sample code to refer then it will be very helpful.
Kindly help me with your valuable suggestions.
Thanks & Regards:-
utpal