Other Parts Discussed in Thread: HALCOGEN, TMS570LS0332
Hi,
Just an FYI. As I am working with mibspi, I noticed a warning is being generated after enabling the mibspi driver. I am using the TMS570LS0332, CCS 6 and Halcogen 4.1. Hopefully this can be addressed in the next release.
The warning is "#188-D pointless comparison of unsigned integer with zero", the code is in mibspiInit
#if (1U > 0U)
{
while (i < (1U-1U))
{
mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U) /* buffer mode */
| (uint16)((uint16)0U << 12U) /* chip select hold */
| (uint16)((uint16)1U << 10U) /* enable WDELAY */
| (uint16)((uint16)0U << 11U) /* lock transmission */
| (uint16)((uint16)0U << 8U) /* data format */
/*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
| ((uint16)(~((uint16)0xFFU ^ (uint16)CS_0)) & (uint16)0x00FFU); /* chip select */
i++;
}
Thanks,
David