This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

No build tools!

Expert 1030 points

Other Parts Discussed in Thread: TM4C1230C3PM, TM4C123GH6PM, MSP-FET

I have downloaded the latest version of SW-TM4C-2.1.0 and installed it, but when I import the TivaWare_C_Series usblib project from the Resource Explorer I get a small red error box in the Project Explorer view. What this means I don't know as none of the 'subdirectories' has an error marker onit. If I right click on the project name and select 'Properties' I see the Tiva variant is a TM4C1230C3PM. If I then try to change the device from a TM4C1230C3PM to what I'm actually using, a TM4C123GH6PM, I get the following error message:

No build tools are currently installed for this device family.

Can anybody tell me what is going wrong here? Also, can anyone tell me if the Tiva series is programmable using an MSP-FET430UIF or must I use the Stellaris In-Circuit Debug Interface. Thanks.