Other Parts Discussed in Thread: LMFLASHPROGRAMMER, TM4C1294NCPDT
Hi all,
My first board came back, but in the first try, TM4C1294 is toasted.
Since I have only ONE spare TM4C1294, and I will not be able to get another one for weeks, so I would like to gather as much information as possible before I replace the IC.
1) Double check all power and ground, check
2) 3.3V supplies the IC, check
3) Manually verify there is nothing higher than 3.3V appears on ALL pins of TM4C1294, check
3) Vddc has 1.2V, check
One possibility, before the power is applied, we accidentally plug in the USB cable, so the 5V reaches TM4C1294's USB0VBUS line earlier than the supply.
Could this 5V on an un-powered TM4C1294 burn out the IC? If so, I will use the spare part and try again
Thanks!