Other Parts Discussed in Thread: HALCOGEN
Hello,
Can I use the generated source code by HalCoGen v4.00 using TMS570LS20216SZWT_FREERTOS project wizard
for TMS570LS20216SPGE device?
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: HALCOGEN
Hello,
Can I use the generated source code by HalCoGen v4.00 using TMS570LS20216SZWT_FREERTOS project wizard
for TMS570LS20216SPGE device?
Regards
Hello,
Yes, you should be able to use the generated source code. You need to be careful to only use I/O functions that are available on both the ZWT as well as the PGE packages. Also, the PGE package has a lower maximum speed specification of 140MHz versus the ZWT package (160MHz). So you will need to configure the PLL in HALCoGen to generate 140MHz instead of 160MHz if you indeed need to use the max clock speeds.
Regards, Sunil
Hello sir,
I have one question
TMS570LS20216SZWT is 337pin board
TMS570LS20216SPGE is 144pin board
by changing PLL from 160 to 140MHz , will lead to working ( that is " FreeRTOS will work on SPGE? ")
So SPGE will support FreeRTOS?, Thank you sir
Regards, Thamizh
Hello,
Yes, you should be able to run the same source code once the system initialization is updated for the change in operating frequency.
Regards, Sunil
P.S.: Please post your question on a new thread as this one is already marked answered and closed.