This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Power led on, connection is ok, but no respond

Hello everyone, I'm really new for microcontrollers although I have some knowledge about c language. Well, the issue is my tiva c tm4c123g board's power led is on (only on led), also Stellaris ICDI DFU device and JTAG/SWD interface and VSP(com6) is ok and I tried CCS and LM flash programmer, they both erase flash and program again without any problem but the program does not run (e.g blinky, led does not blink or hello, I see nothing in the putty at com6 br 115200) I'm not sure but I tried this code accidentally before, a blue led was on because of the running program but then it turned off. The code is on processing

"

import processing.serial.*;
 
PFont font;
int pwmValue;
Serial mySerial;
int serialIndex = 0;
 
void setup() {
  font  = createFont("Arial", 32);
  size(300, 301);
  mySerial = new Serial(this, Serial.list()[serialIndex], 115200);
}
 
void draw() {
  background(200);
  if (mouseY > 44) {
    line(0, mouseY, 300, mouseY);
    pwmValue = int(constrain(-2.1*(mouseY - 172), -255, 255));
    fill(0);
  }
  else {
    pwmValue = 0;
    fill(70);
  }
  rect(0, 0, 300, 44);
  textAlign(LEFT, TOP);
  textFont(font, 16);
  fill(255);
  text("Current Speed: " + str(pwmValue), 9, 9);
  fill(255, 0, 0);
  text("Rollover to Reset", 160, 9);
 
  mySerial.write(str(pwmValue));
  mySerial.write("#");
  mySerial.write(str(pwmValue));
  mySerial.write(10);
}
"
and this code
after

// Graphing sketch


// This program takes ASCII-encoded strings
// from the serial port at 9600 baud and graphs them. It expects values in the
// range 0 to 1023, followed by a newline, or newline and carriage return

// Created 20 Apr 2005
// Updated 18 Jan 2008
// by Tom Igoe
// This example code is in the public domain.

import processing.serial.*;

Serial myPort; // The serial port
int xPos = 1; // horizontal position of the graph
int serialIndex = 0;
void setup () {
// set the window size:
size(400, 300);

// List all the available serial ports
println(Serial.list());
// I know that the first port in the serial list on my mac
// is always my Arduino, so I open Serial.list()[0].
// Open whatever port is the one you're using.
myPort = new Serial(this, Serial.list()[0], 9600);
// don't generate a serialEvent() unless you get a newline character:
myPort.bufferUntil('\n');
// set inital background:
background(0);
}
void draw () {
// everything happens in the serialEvent()
}

void serialEvent (Serial myPort) {
// get the ASCII string:
String inString = myPort.readStringUntil('\n');

if (inString != null) {
// trim off any whitespace:
inString = trim(inString);
// convert to an int and map to the screen height:
float inByte = float(inString);
inByte = map(inByte, 0, 1023, 0, height);

// draw the line:
stroke(127,34,255);
line(xPos, height, xPos, height - inByte);

// at the edge of the screen, go back to the beginning:
if (xPos >= width) {
xPos = 0;
background(0);
}
else {
// increment the horizontal position:
xPos++;
}
}
}