This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

interfacing Tiva launch pad with TFT LCD



Hai,

Please help me to interface TFT LCD with Tiva C launchpad, is there any sample code for TFT LCD?

Thank you

  • Hi sivaprasad,

    There is this, which includes a TFT LCD tutorial:

    http://processors.wiki.ti.com/index.php/Getting_Started_with_the_TIVA%E2%84%A2_C_Series_TM4C123G_LaunchPad

  • sivaprasad sm said:

    Please help me to interface TFT LCD with Tiva C launchpad, is there any sample code for TFT LCD?

     Sample code for TFT is included on software package.

     To interface a specific LCD then more and more information are to be specified. I suggest you to buy a launchpad with LCD and try use the examples that come with them.

     Missing information:

     Launchpad type

     LCD type

     if multimode LCD than serial/parallel mode color depth..

     and so on all parameter of display/controller

  • Thank you guys for your timely help and response,

    I have TM4C123G Launchpad and HY32D TFT LCD  based on SSD1289 display controller, how i can use the grlib for this purpose? is it possible to modify the sample code for this specific module?....

  • sivaprasad sm said:
     based on SSD1289 display controller, how i can use the grlib for this purpose?

     Examples are based on that controller, otherwise other are using that controller and you can see schematic and code from them, try launchpad boosterpack page and see Robg or Dany Rebollo BP LCD.

    http://www.ti.com/ww/en/launchpad/boosterpacks.html

  • sivaprasad sm said:
    Have HY32D TFT LCD  based on SSD1289 display controller

    Wonder how you arrived @ that particular display?  Might a more mainstream (i.e. available, recent tech) TFT prove superior?

    Not all of your cost will be display, alone.  And - if that display proves an, "orphan" or difficult to purchase again - or in quantity - it's selection may be short-sighted.

    Enlightened display vendors provide an integrated "family" of displays - often a design for just "one" proves a design for many.  (sometimes, all!)  Undertaking such design once - rather than uniquely for each new requirement - appeals to many.  Perhaps warrants some consideration...

  • cb1- said:
    Wonder how you arrived @ that particular display?

     I think as I got there by price selection or by ebay:

    http://www.hotmcu.com/32-touch-screen-tft-lcd-with-16-bit-parallel-interface-p-36.html

     having a pcb support the first time interfacing it is a good starting point when low cost boosterpack where not  available like now

  • Roberto Romano said:
    I got there by price selection or by ebay:

    Agree with the advantage of pcb support - however what's, "one day there" @ ebay may not prove the case when you (later) return!  And - rarely do best/brightest displays (and tech support teams) wade ebay waters...

    Figures of merit for displays include; Contrast, Viewing Angle, Backlight brightness & presence/absence of Controller and/or "semi-standard" connector interface. 

    Too often -arts sourced in such manner - are orphans, overstocks, and/or have not proved successful in the "normal" market channels...

    The goal of, "Design Once" then Sell and produce (that initial design) in volume - steers toward more conventional sourcing methods...

  • cb1- said:
    The goal of, "Design Once" then Sell and produce (that initial design) in volume - steers toward more conventional sourcing methods...

     Hi CB1, when I selected this items it was ready to use with simple connection than made custom pcb, after that spare sample I got to conventional for mass production but remember for prototyping this assembly is a bargain.

     In case you wish do production number are good:

    • Model: HY32D
    • Shipping Weight: 60g
    • 592 Units in Stock
    • Manufactured by: HAOYU Electronic

     But I still prefer mass production from a good source ;)

  • Thank you, Roberto.  We'll check the specs on this & report.

    We try to avoid, "Design/develop - then repeat" (for the same project...)   Investors (rightfully) scream!  (cb1 nightmare)