This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fault ISR on portf interrupt

hiiii all,

i enabled falling edge interrupt on port f. there i am counting by timer. now when i use this count outside ISR (i mean in main), program goes in fault ISR. kindly give suggestions.

Regards

prashant

  • Hello Prashant

    A lot of things can go wrong, if we do not know the application code you have written?

    Regards

    Amit

  • #include<inc/tm4c123gh6pm.h>
    #include <stdint.h>
    #include <stdbool.h>
    #include "inc/hw_gpio.h"
    #include "inc/hw_types.h"
    #include "inc/hw_memmap.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/pin_map.h"
    #include "driverlib/gpio.h"
    #include "driverlib/pwm.h"
    #include "driverlib/adc.h"
    #include "driverlib/sysctl.h"
    #include<driverlib/interrupt.h>
    #include<driverlib/timer.h>
    void PortFIntHandler(void);
    void PortFInit(void);
    volatile unsigned long ui32Loop,Count;
    volatile unsigned long Old_Count,Elapsed_Count;
    volatile unsigned long New_Count=0;
    float freq,speed,speedref,error;
    volatile unsigned long ha,hb,hc;
    int main(void){
    	error=0.00;
    	speedref=1200.00;
    	SysCtlClockSet(SYSCTL_SYSDIV_2_5 | SYSCTL_USE_PLL |   SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
    		   SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
    		   SysCtlDelay(3);
    		   SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
    		   SysCtlDelay(3);
    		   SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
    		   SysCtlDelay(3);
    		   GPIOPinTypeGPIOOutput(GPIO_PORTD_BASE, GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);
    		   GPIOPinTypeGPIOOutput(GPIO_PORTE_BASE, GPIO_PIN_1|GPIO_PIN_2);
    		   GPIOPinTypeGPIOInput(GPIO_PORTA_BASE, GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7);
    	SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
    		SysCtlDelay(3);
    		TimerDisable(TIMER0_BASE,TIMER_A);
    		TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC_UP);
    		 TimerLoadSet(TIMER0_BASE, TIMER_A, 0x00FFFFFF);
    		TimerEnable(TIMER0_BASE, TIMER_A);
          PortFInit(); // initialize GPIO Port F interrupt
    
       while(1)
       {
    	   ha=GPIOPinRead(GPIO_PORTA_BASE,GPIO_PIN_5) & 0x20;
    	   	        	   hb=GPIOPinRead(GPIO_PORTA_BASE,GPIO_PIN_6) & 0x40;
    	   	        	   hc=GPIOPinRead(GPIO_PORTA_BASE,GPIO_PIN_7) & 0x80;
    speed=speed+1;
    	   	        	   if(ha==0x20 && hb==0x40 && hc==0x80)  //111
    	   	        	      	      {
    	   	        	      	           	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_1, false);
    	   	        	      	           	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_0, false);
    	   	        	      	           	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_3, false);
    	   	        	      	           	  GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_2, false);
    	   	        	      	           	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_2, false);
    	   	        	      	           	  GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_1, false);
    	   	        	      	           	}
    	   	        	   if(ha!=0x20 && hb!=0x40 && hc!=0x80)  //000
    	   	        	       	      	      {
    	   	        	       	      	           	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_1, false);
    	   	        	       	      	           	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_0, false);
    	   	        	       	      	           	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_3, false);
    	   	        	       	      	           	  GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_2, false);
    	   	        	       	      	           	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_2, false);
    	   	        	       	      	           	  GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_1, false);
    	   	        	       	      	           	}
    	   	        	   if(ha==0x20 && hb==0x40 && hc!=0x80) //110
    	   	        	      {
    	   	        	   	   GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_0, false);
    	   	        	   	   GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_1, false);
    	   	        	   	   GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_2, false);
    	   	        	   	   GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_1, false);
    	   	        	   	   GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_3, GPIO_PIN_3);
    	   	        	   	   GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_2, GPIO_PIN_2);
    	   	        	      }
    	   	        	      if(ha!=0x20 && hb==0x40 && hc!=0x80) //010
    	   	        	      {
    
    
    	   	        	   	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_2, false);
    	   	        	   	  GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_1, false);
    	   	        	   	  GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_2, false);
    	   	        	   	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_1, GPIO_PIN_1);
    	   	        	   	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_3, GPIO_PIN_3);
    	   	        	   	}
    	   	        	      if(ha!=0x20 && hb==0x40 && hc==0x80)  //011
    	   	        	      {
    	   	        	   	   GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_0, false);
    	   	        	   	   GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_2, false);
    	   	        	   	   GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_3, false);
    	   	        	   	   GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_1, false);
    	   	        	   	   GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_1, GPIO_PIN_1);
    	   	        	   	   GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_2, GPIO_PIN_2);
    	   	        	      }
    	   	        	      if(ha!=0x20 && hb!=0x40 && hc==0x80)  //001
    	   	        	      {
    	   	        	     	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_2, false);
    	   	        	     	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_1, false);
    	   	        	     	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_3, false);
    	   	        	     	  GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_1, false);
    	   	        	     	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_0, GPIO_PIN_0);
    	   	        	     	  GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_2, GPIO_PIN_2);
    	   	        	     	}
    	   	        	      if(ha==0x20 && hb!=0x40 && hc==0x80)  //101
    	   	        	      {
    	   	        	        	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_1, false);
    	   	        	        	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_2, false);
    	   	        	        	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_3, false);
    	   	        	        	  GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_2, false);
    	   	        	        	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_0, GPIO_PIN_0);
    	   	        	        	  GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_1, GPIO_PIN_1);
    	   	        	        	}
    	   	        	      if(ha==0x20 && hb!=0x40 && hc!=0x80)  //100
    	   	        	      {
    	   	        	           	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_1, false);
    	   	        	           	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_0, false);
    	   	        	           	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_3, false);
    	   	        	           	  GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_2, false);
    	   	        	           	  GPIOPinWrite(GPIO_PORTD_BASE,GPIO_PIN_2, GPIO_PIN_2);
    	   	        	           	  GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_1, GPIO_PIN_1);
    	   	        	           	}
       }
    }
    void PortFInit(void){
    	SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
    	SysCtlDelay(3);
    	GPIOPinTypeGPIOInput(GPIO_PORTF_BASE,GPIO_PIN_4);
    	GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE,GPIO_PIN_3);
    	GPIO_PORTF_PUR_R |= 0x10;     //     enable weak pull-up on PF4
    	GPIOIntTypeSet(GPIO_PORTF_BASE,GPIO_PIN_4,GPIO_FALLING_EDGE);
    	IntEnable(INT_GPIOF);
    	GPIOIntEnable(GPIO_PORTF_BASE, GPIO_INT_PIN_4);
    }
    
    void PortFIntHandler(void){
      GPIO_PORTF_ICR_R = 0x10;      // acknowledge flag4
      Old_Count=New_Count;
        New_Count=TimerValueGet(TIMER0_BASE, TIMER_A);
        if(New_Count>Old_Count)
        {
        Elapsed_Count=New_Count-Old_Count;
        freq=79901869.00/Elapsed_Count;
        speed=freq*15.00;
        }
    }
    

    hiii amit

    i have attached file.

    regards

    prashant

  • Hello Prashant,

    Thanks for the code. I was expecting some sort of explanation as to what works and what does not work.

    I can spend all day understanding the code, and not have an answer. So help from you in explaining (comment in code most welcome) will be useful.

    Regards

    Amit

  • hiii amit
    this is my simplified code. whenever i use any variable from ISR, it enters in fault ISR. here all variables are global variable.
    //a square wave input is given to PortF pin 4. this program measures input signal frequency. int main(void){ SysCtlClockSet(SYSCTL_SYSDIV_2_5 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ); //timer initialization SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0); SysCtlDelay(3); TimerDisable(TIMER0_BASE,TIMER_A); TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC_UP); TimerLoadSet(TIMER0_BASE, TIMER_A, 0x00FFFFFF); TimerEnable(TIMER0_BASE, TIMER_A); PortFInit(); // initialize GPIO Port F interrupt while(1) { speed=freq*15.00; //when i dont use this line, code works } } void PortFInit(void){ SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF); SysCtlDelay(3); GPIOPinTypeGPIOInput(GPIO_PORTF_BASE,GPIO_PIN_4); GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE,GPIO_PIN_3); GPIO_PORTF_PUR_R |= 0x10; // enable weak pull-up on PF4 GPIOIntTypeSet(GPIO_PORTF_BASE,GPIO_PIN_4,GPIO_FALLING_EDGE); IntEnable(INT_GPIOF); GPIOIntEnable(GPIO_PORTF_BASE, GPIO_INT_PIN_4); } void PortFIntHandler(void){ GPIO_PORTF_ICR_R = 0x10; // acknowledge flag4 Old_Count=New_Count; New_Count=TimerValueGet(TIMER0_BASE, TIMER_A); if(New_Count>Old_Count) { Elapsed_Count=New_Count-Old_Count; freq=79901869.00/Elapsed_Count; } }

    regards

    prashant

  • Hello Prashant,

    I hope you realize that the Timer will roll over and it could be possible that the New_Count can be less than Old_Count yielding a -ve number. When the Fault does occur did you check what the value for the two variables. Does it occur on the very first computation or it happens randomly?

    Regards

    Amit

  • Hi  Amit

    I know that the timer will roll over, thats why i used an "if condition" there. and also at the very first time if it gives negative value, whats the problem. actually when i calculated "freq" in portf ISR the program is working fine. but when i use that variable in mains, it goes in ISR. it is happening at very first time itself. can we use a variable outside ISR? it is a global variable.

    Thanks

    Prashant

  • Hello Prashant,

    Attached is the file I have used from your code. I am using the TM4C123 LaunchPad, so use the SW1 to generate the Pulses and after trying for more than 2 minutes of presses, I could not get it to Fault Handler.

    Also since you intend to use float values, I would suggest that you enable the FPU as well.

    Lastly, assume the condition where the value rolled over twice and the NewValue is greated than OldValue. In this case the computation "logically" is incorrect. You have no mechanism in place to detect the same. I can understand the case where the input pulse is like 1MHz and this condition will not happen, but the code should have more fail safes than just a single if condition.

    Regards

    Amit

  • Hii amit,

    sorry for late response. Did you use any variable in Main() which was calculated in ISR? i enabled FPU as well but it is not working at all. same problem.

    regards prashant

  • Hello Prashant,

    I used the program just as you had sent in the first post

    Regards

    Amit

  • Hii amit.

    let me explain you a bit more. I am giving a pulse to PA5. and giving same pulse to PF4. now i am calculating frequency by  portF interrupt handler. but you are giving a single pulse to PF4 (switch press). So for you its working but in my case it is not working. what may be the reason? sorry for inconvenience caused by me.

    thanks

    regards

    prashant 

  • Hello Prashant,

    What is the frequency of the pulses? If the idea is to measure the Pulse Frequency then wouldn't it be better to use the Timer in Input Edge Time Mode.

    Following Recent Post meant to do the same.

    http://e2e.ti.com/support/microcontrollers/tiva_arm/f/908/t/374380.aspx

    Regards

    Amit

  • hii amit

    frequency of the pulses in 300Hz. but i found that problem is different. I am using a floating point variable in if else condition. but now i tried again by converting them into unsigned long. program is going in fault ISR. but i found something interesting. when i run program using "step into" it works perfectly fine. what may be the problem?

    speedref=1000.00;
    hh=(int)speedref;
    if(hh!=3000)
    {
    a=1;
    }

    regards

    prashant

  • Hello Prashant

    What is the NVIC_FAULTSTAT and NVIC_FAULTADDR values when the Fault ISR is executed?

    Regards

    Amit

  • hii amit

    NVIC_FAULTSTAT = 0x40000000

    NVIC_HFAULT_STAT_FORCED = 1 other two are zero

    NVIC_FAULTADDR = 0xE000EDF8

    prashant

  • Hello Prashant,

    The bit in the NVIC_FAULTSTAT that you have mentioned is a reserved bit. It cannot be set. Are you sure that it is address 0xE000ED28.

    Regards

    Amit