Other Parts Discussed in Thread: TLC5940, ENERGIA
d i would like to design a 8x8 matrix display which can be used to display any language or image using TLC 5940.which micro controller is best suited for this application?(Tiva series is ok?)
when i google about this i can understand that there is two lines are used. common line and access line. in which common line is connected to the shift register.if this is correct then my doubts is that whether the shift register shift only one bit at a time?
another one doubts is that using one tlc5940 and one shift register what is the maximum size of display wich can be designed?