This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

connecting TM4C123 with XDS100V2

Hello,

I am designing a custom board with a TM4C123.
I want to program this microcontroller with a XDS100V2 JTAG emulator from SPECTRUM DIGITAL.
The JTAG connector has 14 pins.

Can you tell me if my JTAG connections are OK?

1    connected directly to the TMS pin of the TM4C123
2    connected directly to the RST pin of the TM4C123
3    connected directly to the TDI pin of the TM4C123
4    GND
5    3.3V(TM4C123 supply)
6    leave unconnected
7    connected directly to the TDO pin of the TM4C123


8    GND
9    leave unconnected
10    GND
11    connected directly to the TDK pin of the TM4C123
12    GND
13    leave unconnected
14    leave unconnected

Thanks