Other Parts Discussed in Thread: ENERGIA
Does anybody knows of a forthcoming or existing Simulink support for the TM4C123G or 129 launchpad kits?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ENERGIA
Does anybody knows of a forthcoming or existing Simulink support for the TM4C123G or 129 launchpad kits?
Hello Izhak
Matlab should have the information as it mentions that it supports TIVA platform
Regards
Amit
thank you,
Matlab goes halfway as it supports the specific ARM core, but does not offer Simulink integration like ST32 discovery.
I know that ST produced simulink blocks for the st32 discovery which increased their sales considerably.
it is mu humble opinion that TI could do something too :-)
That is IMHO in correct, that the mathlab support for a MCU has to come trom the vendor - TI in this case.
And you are correct about ST. Microchip did it also, down to their 16-Bit devices (PIC24). Certain branches (like automotive) love it ...
Hello All,
Thanks for the inputs. I would need to see if there is something we can develop as an infrastructure to Tiva product line.
Regards
Amit
Hello Amit,
perhaps you might get inpired here :)
www.mathworks.com/.../37825-simulink--embedded-coder--target-for-ti-launchpad
There is definitely a demand for such a thing, especially from universities side...
Regards
MArtin
Hello Amit,
thanks for the reply.... :)
It is just than numerous people would highly appreciate
such an endevour from the TI side
(just as it happened with C2000 series).
Keep up the good work guys !!!
Best Regards,
Martin