Other Parts Discussed in Thread: TM4C129DNCPDT
Hi,
In my work, i am writing my two application's binary images at two different memory locations in the flash memory. One of the binary resides in the upper half of the flash and other one in lower half. Both the binaries are programmed to blink a different colored LED continuously. Now i am copying the binary from upper half of the flash memory to other(lower half of the flash memory) and jumping to the bootsection of lower half of the flash memory and i can see that the copied image runs successfully. Now i wanted to make sure that even if i now erase the image present in the upper half of the flash memory(which is already copied in the lower half), it should not create any impact on execution of the binary present at lower half. But, that's not happening. When i copy the flash image present in upper half of the flash to lower half addres of the flash memory, and then erase the binary present in the upper half, and then jump to the boot section of the lower image meomory, it ends up in a hard fault. I am not getting why?
I am using Tiva series TM4C129DNCPDT as a controller on my board with XDS200 usb emulator.
Here are the details of what i am actually doing:
1) I have a blinky application which blinks red colored LED on my board continuously. It is flashed at address 0x84000 on the flash memory. Please find the attached linker command file for it in the text format above.
2) Then i have my bootloader binary(5KB in size) copied at address 0x80000 on the flash memory
3) Then i have a binky application which blinks green colored LED on my board continuously. It is flashed at address 0x4000 on the flash memory. Please find the attached linker command file for it in the text format above.
4) Then start debugging the bootloader code (who's binary is also present in the star addres of the upper half of the flash), which starts at address 0x00.
Here is a snapshot of what my boot loader code is doing:
int main(void)
{
set_up_modules();
/* Test copy_flash_image functionality */
copy_flash_image(0x4000, 0x84000, 9216);
erase_bad_image_flash_memory(0x84000, 9216);
__asm(" mov R0, #0x8000");
__asm(" mov PC, r0\n"
" bx r0\n"); }
I can see that the memory location 0x4000 onwards are getting erased and written by the data present at memory location 0x84000, but after that when i erase the memory contents of 0x84000, and then jumps to the boot section of the lower half of memory, it ends up in a segmentation fault.
I am not able to reason it out like why it is happening and need some expert's help on this.
Please have a look and help me on this.
Thanks in advance.
Regards,
Shrikant
#define APP_BASE 0x00084000
#define RAM_BASE 0x20000000
--retain=g_pfnVectors
MEMORY
{
FLASH (RX) : origin = APP_BASE, length = 0x00100000
SRAM (RWX) : origin = 0x20000000, length = 0x00040000
}
/* The following command line options are set as part of the CCS project. */
/* If you are building using the command line, or for some reason want to */
/* define them here, you can uncomment and modify these lines as needed. */
/* If you are using CCS for building, it is probably better to make any such */
/* modifications in your CCS project and leave this file alone. */
/* */
/* --heap_size=0 */
/* --stack_size=256 */
/* --library=rtsv7M4_T_le_eabi.lib */
/* Section allocation in memory */
SECTIONS
{
boot_section > 0x88000
{
-l rtsv7M4_T_le_v4SPD16_eabi.lib<boot.obj>(.text)
}
.intvecs: > APP_BASE
.text : > FLASH
.const : > FLASH
.cinit : > FLASH
.pinit : > FLASH
.init_array : > FLASH
.vtable : > RAM_BASE
.data : > SRAM
.bss : > SRAM
.sysmem : > SRAM
.stack : > SRAM
}
__STACK_TOP = __stack + 512;
#define APP_BASE 0x00004000
#define RAM_BASE 0x20000000
--retain=g_pfnVectors
MEMORY
{
FLASH (RX) : origin = APP_BASE, length = 0x00100000
SRAM (RWX) : origin = 0x20000000, length = 0x00040000
}
/* The following command line options are set as part of the CCS project. */
/* If you are building using the command line, or for some reason want to */
/* define them here, you can uncomment and modify these lines as needed. */
/* If you are using CCS for building, it is probably better to make any such */
/* modifications in your CCS project and leave this file alone. */
/* */
/* --heap_size=0 */
/* --stack_size=256 */
/* --library=rtsv7M4_T_le_eabi.lib */
/* Section allocation in memory */
SECTIONS
{
boot_section > 0x8000
{
-l rtsv7M4_T_le_v4SPD16_eabi.lib<boot.obj>(.text)
}
.intvecs: > APP_BASE
.text : > FLASH
.const : > FLASH
.cinit : > FLASH
.pinit : > FLASH
.init_array : > FLASH
.vtable : > RAM_BASE
.data : > SRAM
.bss : > SRAM
.sysmem : > SRAM
.stack : > SRAM
}
__STACK_TOP = __stack + 512;