This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDS100/XDS200 programmer and compact 20-pin connector

Other Parts Discussed in Thread: TM4C129CNCPDT

I have been asked to specify a programmer for our boards based on TIVA TM4C129 (namely TM4C129CNCPDT). The debug connector in our boards is compatible with the Cortex Debug+ETM connector (as seen in this document: http://infocenter.arm.com/help/topic/com.arm.doc.faqs/attached/13634/cortex_debug_connectors.pdf )

In fact the J1 debug connector in TIVA DK-TM4C129X development board is compatible with this connector (except for the trace connections).

Looking at XDS* programmers pages it seems to me that neither come with a compatible emulation cable, only  the 14-pin TI or the 20-pin TI (whose rows are 0.1" apart, not 0.05") or the legacy 20-pin ARM (0.1" pace).

Is there an off-the-shelf adapter that allow me to connect one of these programmers to my connector? Preferably from the same source as the programmers?


If not, would you suggest an alternative (preferably low cost) programmer?

Thank you in advance.