This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using Tiva c series MCU's USB for displaying

Hi All,


We are using Tiva C series MCU in our application and want to display some parameters which is stored in EEPROM on PC through the USB cable which is connected to our development board(same usb is also giving power to the development board). We already tried the UART and it is working fine (modified the code of UART echo example from TI.

And one more thing is that in hyperterminal we use to select the COMP port while doing the UART echo example for display but now if we see in device manger our board is reflecting as a "Stellaris Deivce Firmware Upgrade" and not as any COMP port.

So any one please help me to resolve this and also please share the example code if any.

Any help is greatly appreciated.

Thanks and regards,

Sreenivasa S