Other Parts Discussed in Thread: TM4C1231H6PM, TM4C123GH6PM
I tried to configure an adc interrupt when the pwm1 generates the zero signal. The trigger from the pwm never wakes the adc. It's strange, when I triggered the adc with adc trigger processor it works. I already modified my tm4c1231h6pm_startup_ccs.c file.
This is my code. I tried everything
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"
#include "driverlib/debug.h"
#include "driverlib/pwm.h"
#include "driverlib/pin_map.h"
#include "inc/hw_gpio.h"
#include "driverlib/rom.h"
#include "inc/tm4c123gh6pm.h"
#include "driverlib/adc.h"
#include "driverlib/interrupt.h"
#define PWM_FREQUENCY 60
uint32_t muestrasPot[4]={0,0,0,0};
int main(void)
{
volatile uint32_t ui32Load;
volatile uint32_t ui32PWMClock;
volatile uint8_t ui8Adjust;
ui8Adjust = 45;
ROM_SysCtlClockSet(SYSCTL_SYSDIV_2_5|SYSCTL_USE_PLL|SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ);
ROM_SysCtlPWMClockSet(SYSCTL_PWMDIV_64);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM1);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_2 |GPIO_PIN_3);
ROM_GPIOPinTypePWM(GPIO_PORTD_BASE, GPIO_PIN_0);
ROM_GPIOPinConfigure(GPIO_PD0_M1PWM0);
HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
HWREG(GPIO_PORTF_BASE + GPIO_O_CR) |= 0x01;
HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = 0;
ROM_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_5);
ROM_ADCReferenceSet(ADC0_BASE, ADC_REF_INT);
ROM_ADCSequenceConfigure(ADC0_BASE, 1, ADC_TRIGGER_PWM0|ADC_TRIGGER_PWM_MOD1, 0);
ROM_ADCSequenceStepConfigure(ADC0_BASE, 1, 0, ADC_CTL_CH8);
ROM_ADCSequenceStepConfigure(ADC0_BASE, 1, 1, ADC_CTL_CH8);
ROM_ADCSequenceStepConfigure(ADC0_BASE, 1, 2, ADC_CTL_CH8);
ROM_ADCSequenceStepConfigure(ADC0_BASE, 1, 3, ADC_CTL_CH8|ADC_CTL_IE|ADC_CTL_END);
ROM_ADCSequenceEnable(ADC0_BASE, 1);
ROM_GPIODirModeSet(GPIO_PORTF_BASE, GPIO_PIN_4|GPIO_PIN_0, GPIO_DIR_MODE_IN);
ROM_GPIOPadConfigSet(GPIO_PORTF_BASE, GPIO_PIN_4|GPIO_PIN_0, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU);
ui32PWMClock = ROM_SysCtlClockGet() / 64;
ui32Load = (ui32PWMClock / PWM_FREQUENCY) - 1;
ROM_PWMGenConfigure(PWM1_BASE, PWM_GEN_0, PWM_GEN_MODE_DOWN);
ROM_PWMGenPeriodSet(PWM1_BASE, PWM_GEN_0, ui32Load);
ROM_PWMPulseWidthSet(PWM1_BASE, PWM_OUT_0, ui8Adjust * ui32Load / 1000);
ROM_PWMOutputState(PWM1_BASE, PWM_OUT_0_BIT, true);
ROM_PWMGenEnable(PWM1_BASE, PWM_GEN_0);
ROM_PWMGenIntTrigEnable(PWM1_BASE, PWM_GEN_0, PWM_TR_CNT_ZERO);
ROM_ADCIntEnable(ADC0_BASE, 1);
ROM_IntEnable(INT_ADC0SS1);
ROM_ADCIntClear(ADC0_BASE, 1);
ROM_IntMasterEnable();
while(1)
{
}
}
void ADCSeq1IntHandler(void)
{
ADCIntClear(ADC0_BASE, 1);
ADCSequenceDataGet(ADC0_BASE, 1, muestrasPot);
}