Other Parts Discussed in Thread: TM4C123GH6PM
Hi, I’m using the tm4c123gh6pm lauchpad, and I’m trying to activate the SPI. The SSI0 is working perfect, I can see all the signals in my logic analyzer. However I need to use the SSI2 because the pinout I need. When I configure SSI2, I can see SS2Tx in my logic analyzer, but there is no clock output! I realized that PB4 share functionality with AIN10 maybe I need to do an extra configuration somebody can help me?
Regards.