This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPNZ195D Errata ADC#1

Hello,

One workaround for this errata is:

"Limit the analog input upper limit to be lower than (VDDA - 0.3V)."

Is VDDA the same as VCCAD?

Also - the two figures have black text on black background - I assume they should look like the ones supplied in this thread:

http://e2e.ti.com/support/microcontrollers/hercules/f/312/t/314565.aspx

Thanks, Charlie Johnston

  • Charlie,

    Yes, VCCAD is the correct name.   Sometimes we refer to it as VDDA internally and this creeped into the errata.

    Sorry about the picture being blacked out.  That really isn't acceptable.  I believe it should be the same image that Sunil posted but I am assigning this to Sunil to confirm since he is sourcing the errrata information for this issue.


    Sunil, were there any changes between the posted version of the PDF http://e2e.ti.com/support/microcontrollers/hercules/f/312/t/314565.aspx and what you sourced for the errata? 

     

  • Hi Anthony,

    Another clarification:

    "Limit the analog input upper limit to be lower than (VDDA - 0.3V)."

    Does this refer to the unique input, the shared input, or both?

    Thanks, Charlie

  • Charlie,

    My understanding is that the shared input channels need to be limited in input voltage range otherwise they could affect the conversion result of (any) channel on the other ADC. 

    But I asked Sunil to comment on this thread and he is the best person to also confirm this point.

  • Anthony,

    Yes, the issue is caused by injecting current into the shared-input channel. The workaround also requires that the input level on the shared-input channel be limited to (VDDA - 0.3V). We will make this update to the description in the errata documents.

    As for the image, it was supposed to be identical to what I had posted on the related forum thread. Need to check what happened to the color scheme and correct it.

    Regards, Sunil