Other Parts Discussed in Thread: HALCOGEN
Hi,
I am having a few issues with halcogen 4.0.0 on the RM48 at the moment.
These being ECLK configuration. We configure this via halcogen and generate code. This code works giving us our ECLK output. On exit and then rentry to halcogen we loose this setting and it reverts back to GIO. This means developers using halcogen are inadvertently turning off our ECLK.
Also we want to use V10 as an output for MISBSPI3NCS0 as a GIO output. Yet the pinmux configuration for this pin is grayed out and configured to GIOB2.
Anyone come across these issues?
Do I have to manually edit halcogen code to get around the V10 issue?
Have I missed some critical config within halgocogen that is necessary for the configuration of ECLK and pin V10 configuration?
Regards,
Owain