Other Parts Discussed in Thread: TM4C123GH6PZ
Hi.I'm using the TM4C123GH6PZ controller with 8MHZ external crystal frequency.I have set My system clock is 8MHZ.
i'm giving the pulses to PB4 (frequency range is 1K to 10K HZ).now in need to capture the pulse with in certain period of time..so i'm using the two timers for this application
i'm using the timer0 for creating one second delay with an interrupt.when interrupt will generate then i'm going to count the pulse using timer 2 .Is this the correct way to do it like this???
please help me
thank sin advance.