I have been struggling for a while with trying to get my TIVA part to communicate reliably with another IC on my custom board. I connected a logic analyzer and an o'scope to evaluate the SCL and SDA lines. My first move was to change the pull-up resistors to get better looking waveforms. After that, everything looked good - the logic analyzer was showing what I was sending, but I was still not getting reliable communication.
I then realized that SCL was running at 1 MHz. WTH? I called I2CMasterInitExpClk correctly (I think):
I2CMasterInitExpClk(I2C1_BASE, SysCtlClockGet(), false);
The documentation states that this should give a 100 KHz clock.
I then looked within the I2CMasterInitExpClk code and found this:
// Compute the clock divider that achieves the fastest speed less than or
// equal to the desired speed. The numerator is biased to favor a larger
// clock divider so that the resulting clock is always less than or equal
// to the desired clock, never greater.
//
ui32TPR = ((ui32I2CClk + (2 * 10 * ui32SCLFreq) - 1) /
(2 * 10 * ui32SCLFreq)) - 1;
HWREG(ui32Base + I2C_O_MTPR) = ui32TPR;
//
// Check to see if this I2C peripheral is High-Speed enabled. If yes, also
// choose the fastest speed that is less than or equal to 3.4 Mbps.
//
if(HWREG(ui32Base + I2C_O_PP) & I2C_PP_HS)
{
ui32TPR = ((ui32I2CClk + (2 * 3 * 3400000) - 1) /
(2 * 3 * 3400000)) - 1;
HWREG(ui32Base + I2C_O_MTPR) = I2C_MTPR_HS | ui32TPR;
}
So it looks to me that things are setup to be the fastest clock under 3.4 Mbps.
If I manually change the I2C_O_MTPR register to 0x0A, SCL then runs at 500KHz and my communication is reliable.
What am I missing?
Thanks,
Jeff