This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Launchpad USB HID keyboard example stucks



Hi,

I'd like to transfer the dk-tm4c123g usb device keyboard example to my Tiva-C Launchpad. I modified the pin configurations according to my mcu and successfully compiled the project. The PC recognizes the hardware as 'Keyboard Example' keyboard and the hardware reflects the state of the caps lock button. However, the execution stucks at 

//
        // Wait here until USB device is connected to a host.
        //
        while(!g_bConnected)
        {
        }

and never gets further. I placed a couple of LED outputs in the code for test purposes which has showed me that the connected state had been reached and never got disconnected (red LED is on continuously). It seems that the code execution won't reach the 

UARTprintf("Host connected...\n");

part of the code and by stopping the execution using the debugger, the code seems to be stucked in the NextConfigDescGet function which has no source file associated. I attached my code below.

Any help would be greatly welcome since I'm out of ideas at the moment.

Update: In some random cases the board was able to send the expected string (minus the last character '!' which is the ' character (quotation) strangely) to the PC. It is rather strange since the code had not been changed at all. Maybe it is related to the unused USB Vbus and ID pins?

Update2: The '!' character is exchanged to ' probably because of the differing keyboard layout.

//*****************************************************************************
//
// usb_dev_keyboard.c - Main routines for the keyboard example.
//
// Copyright (c) 2011-2014 Texas Instruments Incorporated.  All rights reserved.
// Software License Agreement
// 
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
// 
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
// 
// This is part of revision 2.1.0.12573 of the DK-TM4C123G Firmware Package.
//
//*****************************************************************************

#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_gpio.h"
#include "inc/hw_sysctl.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/uart.h"
#include "usblib/usblib.h"
#include "usblib/usbhid.h"
#include "usblib/device/usbdevice.h"
#include "usblib/device/usbdhid.h"
#include "usblib/device/usbdhidkeyb.h"
#include "utils/uartstdio.h"

#include "drivers/buttons.h"
#include "usb_keyb_structs.h"


//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>USB HID Keyboard Device (usb_dev_keyboard)</h1>
//!
//! This example application turns the evaluation board into a USB keyboard
//! supporting the Human Interface Device class.  When the push button is
//! pressed, a sequence of key presses is simulated to type a string.  Care
//! should be taken to ensure that the active window can safely receive the
//! text; enter is not pressed at any point so no actions are attempted by the
//! host if a terminal window is used (for example).  The status LED is used to
//! indicate the current Caps Lock state and is updated in response to any
//! other keyboard attached to the same USB host system.
//!
//! The device implemented by this application also supports USB remote wakeup
//! allowing it to request the host to reactivate a suspended bus.  If the bus
//! is suspended (as indicated on the application display), pressing the
//! push button will request a remote wakeup assuming the host has not
//! specifically disabled such requests.
//
//*****************************************************************************

//*****************************************************************************
//
// The system tick timer period.
//
//*****************************************************************************
#define SYSTICKS_PER_SECOND     100

//*****************************************************************************
//
// A mapping from the ASCII value received from the UART to the corresponding
// USB HID usage code.
//
//*****************************************************************************
static const int8_t g_ppi8KeyUsageCodes[][2] =
{
    { 0, HID_KEYB_USAGE_SPACE },                       //   0x20
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_1 },         // ! 0x21
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_FQUOTE },    // " 0x22
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_3 },         // # 0x23
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_4 },         // $ 0x24
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_5 },         // % 0x25
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_7 },         // & 0x26
    { 0, HID_KEYB_USAGE_FQUOTE },                      // ' 0x27
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_9 },         // ( 0x28
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_0 },         // ) 0x29
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_8 },         // * 0x2a
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_EQUAL },     // + 0x2b
    { 0, HID_KEYB_USAGE_COMMA },                       // , 0x2c
    { 0, HID_KEYB_USAGE_MINUS },                       // - 0x2d
    { 0, HID_KEYB_USAGE_PERIOD },                      // . 0x2e
    { 0, HID_KEYB_USAGE_FSLASH },                      // / 0x2f
    { 0, HID_KEYB_USAGE_0 },                           // 0 0x30
    { 0, HID_KEYB_USAGE_1 },                           // 1 0x31
    { 0, HID_KEYB_USAGE_2 },                           // 2 0x32
    { 0, HID_KEYB_USAGE_3 },                           // 3 0x33
    { 0, HID_KEYB_USAGE_4 },                           // 4 0x34
    { 0, HID_KEYB_USAGE_5 },                           // 5 0x35
    { 0, HID_KEYB_USAGE_6 },                           // 6 0x36
    { 0, HID_KEYB_USAGE_7 },                           // 7 0x37
    { 0, HID_KEYB_USAGE_8 },                           // 8 0x38
    { 0, HID_KEYB_USAGE_9 },                           // 9 0x39
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_SEMICOLON }, // : 0x3a
    { 0, HID_KEYB_USAGE_SEMICOLON },                   // ; 0x3b
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_COMMA },     // < 0x3c
    { 0, HID_KEYB_USAGE_EQUAL },                       // = 0x3d
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_PERIOD },    // > 0x3e
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_FSLASH },    // ? 0x3f
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_2 },         // @ 0x40
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_A },         // A 0x41
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_B },         // B 0x42
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_C },         // C 0x43
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_D },         // D 0x44
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_E },         // E 0x45
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_F },         // F 0x46
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_G },         // G 0x47
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_H },         // H 0x48
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_I },         // I 0x49
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_J },         // J 0x4a
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_K },         // K 0x4b
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_L },         // L 0x4c
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_M },         // M 0x4d
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_N },         // N 0x4e
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_O },         // O 0x4f
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_P },         // P 0x50
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_Q },         // Q 0x51
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_R },         // R 0x52
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_S },         // S 0x53
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_T },         // T 0x54
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_U },         // U 0x55
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_V },         // V 0x56
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_W },         // W 0x57
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_X },         // X 0x58
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_Y },         // Y 0x59
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_Z },         // Z 0x5a
    { 0, HID_KEYB_USAGE_LBRACKET },                    // [ 0x5b
    { 0, HID_KEYB_USAGE_BSLASH },                      // \ 0x5c
    { 0, HID_KEYB_USAGE_RBRACKET },                    // ] 0x5d
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_6 },         // ^ 0x5e
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_MINUS },     // _ 0x5f
    { 0, HID_KEYB_USAGE_BQUOTE },                      // ` 0x60
    { 0, HID_KEYB_USAGE_A },                           // a 0x61
    { 0, HID_KEYB_USAGE_B },                           // b 0x62
    { 0, HID_KEYB_USAGE_C },                           // c 0x63
    { 0, HID_KEYB_USAGE_D },                           // d 0x64
    { 0, HID_KEYB_USAGE_E },                           // e 0x65
    { 0, HID_KEYB_USAGE_F },                           // f 0x66
    { 0, HID_KEYB_USAGE_G },                           // g 0x67
    { 0, HID_KEYB_USAGE_H },                           // h 0x68
    { 0, HID_KEYB_USAGE_I },                           // i 0x69
    { 0, HID_KEYB_USAGE_J },                           // j 0x6a
    { 0, HID_KEYB_USAGE_K },                           // k 0x6b
    { 0, HID_KEYB_USAGE_L },                           // l 0x6c
    { 0, HID_KEYB_USAGE_M },                           // m 0x6d
    { 0, HID_KEYB_USAGE_N },                           // n 0x6e
    { 0, HID_KEYB_USAGE_O },                           // o 0x6f
    { 0, HID_KEYB_USAGE_P },                           // p 0x70
    { 0, HID_KEYB_USAGE_Q },                           // q 0x71
    { 0, HID_KEYB_USAGE_R },                           // r 0x72
    { 0, HID_KEYB_USAGE_S },                           // s 0x73
    { 0, HID_KEYB_USAGE_T },                           // t 0x74
    { 0, HID_KEYB_USAGE_U },                           // u 0x75
    { 0, HID_KEYB_USAGE_V },                           // v 0x76
    { 0, HID_KEYB_USAGE_W },                           // w 0x77
    { 0, HID_KEYB_USAGE_X },                           // x 0x78
    { 0, HID_KEYB_USAGE_Y },                           // y 0x79
    { 0, HID_KEYB_USAGE_Z },                           // z 0x7a
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_LBRACKET },  // { 0x7b
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_BSLASH },    // | 0x7c
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_RBRACKET },  // } 0x7d
    { HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_BQUOTE },    // ~ 0x7e
};

//*****************************************************************************
//
// This global indicates whether or not we are connected to a USB host.
//
//*****************************************************************************
volatile bool g_bConnected = false;

//*****************************************************************************
//
// This global indicates whether or not the USB bus is currently in the suspend
// state.
//
//*****************************************************************************
volatile bool g_bSuspended = false;

//*****************************************************************************
//
// Global system tick counter holds elapsed time since the application started
// expressed in 100ths of a second.
//
//*****************************************************************************
volatile uint32_t g_ui32SysTickCount;

//*****************************************************************************
//
// The number of system ticks to wait for each USB packet to be sent before
// we assume the host has disconnected.  The value 50 equates to half a second.
//
//*****************************************************************************
#define MAX_SEND_DELAY          50

//*****************************************************************************
//
// This global is set to true if the host sends a request to set or clear
// any keyboard LED.
//
//*****************************************************************************
volatile bool g_bDisplayUpdateRequired;

//*****************************************************************************
//
// This enumeration holds the various states that the keyboard can be in during
// normal operation.
//
//*****************************************************************************
volatile enum
{
    //
    // Unconfigured.
    //
    STATE_UNCONFIGURED,

    //
    // No keys to send and not waiting on data.
    //
    STATE_IDLE,

    //
    // Waiting on data to be sent out.
    //
    STATE_SENDING
}
g_eKeyboardState = STATE_UNCONFIGURED;

//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif

//*****************************************************************************
//
// Handles asynchronous events from the HID keyboard driver.
//
// \param pvCBData is the event callback pointer provided during
// USBDHIDKeyboardInit().  This is a pointer to our keyboard device structure
// (&g_sKeyboardDevice).
// \param ui32Event identifies the event we are being called back for.
// \param ui32MsgData is an event-specific value.
// \param pvMsgData is an event-specific pointer.
//
// This function is called by the HID keyboard driver to inform the application
// of particular asynchronous events related to operation of the keyboard HID
// device.
//
// \return Returns 0 in all cases.
//
//*****************************************************************************
uint32_t
KeyboardHandler(void *pvCBData, uint32_t ui32Event, uint32_t ui32MsgData,
                void *pvMsgData)
{
    switch (ui32Event)
    {
        //
        // The host has connected to us and configured the device.
        //
        case USB_EVENT_CONNECTED:
        {
            g_bConnected = true;
            g_bSuspended = false;
            ROM_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, GPIO_PIN_1);
            break;
        }

        //
        // The host has disconnected from us.
        //
        case USB_EVENT_DISCONNECTED:
        {
            g_bConnected = false;
            ROM_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, 0);
            break;
        }

        //
        // We receive this event every time the host acknowledges transmission
        // of a report. It is used here purely as a way of determining whether
        // the host is still talking to us or not.
        //
        case USB_EVENT_TX_COMPLETE:
        {
        	int i = 0;
            //
            // Enter the idle state since we finished sending something.
            //
            g_eKeyboardState = STATE_IDLE;
            ROM_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_3, GPIO_PIN_3);
            for (;i < 100000; ++i)
            	;
            ROM_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_3, 0);
            break;
        }

        //
        // This event indicates that the host has suspended the USB bus.
        //
        case USB_EVENT_SUSPEND:
        {
            g_bSuspended = true;
            ROM_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, GPIO_PIN_2);
            break;
        }

        //
        // This event signals that the host has resumed signalling on the bus.
        //
        case USB_EVENT_RESUME:
        {
            g_bSuspended = false;
            break;
        }

        //
        // This event indicates that the host has sent us an Output or
        // Feature report and that the report is now in the buffer we provided
        // on the previous USBD_HID_EVENT_GET_REPORT_BUFFER callback.
        //
        case USBD_HID_KEYB_EVENT_SET_LEDS:
        {
            //
            // Set the LED to match the current state of the caps lock LED.
            //
            ROM_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2,
                             (ui32MsgData & HID_KEYB_CAPS_LOCK) ? GPIO_PIN_2 :
                             0);

            break;
        }

        //
        // We ignore all other events.
        //
        default:
        {
            break;
        }
    }

    return(0);
}

//***************************************************************************
//
// Wait for a period of time for the state to become idle.
//
// \param ui32TimeoutTick is the number of system ticks to wait before
// declaring a timeout and returning \b false.
//
// This function polls the current keyboard state for ui32TimeoutTicks system
// ticks waiting for it to become idle.  If the state becomes idle, the
// function returns true.  If it ui32TimeoutTicks occur prior to the state
// becoming idle, false is returned to indicate a timeout.
//
// \return Returns \b true on success or \b false on timeout.
//
//***************************************************************************
bool
WaitForSendIdle(uint_fast32_t ui32TimeoutTicks)
{
    uint32_t ui32Start;
    uint32_t ui32Now;
    uint32_t ui32Elapsed;

    ui32Start = g_ui32SysTickCount;
    ui32Elapsed = 0;

    while(ui32Elapsed < ui32TimeoutTicks)
    {
        //
        // Is the keyboard is idle, return immediately.
        //
        if(g_eKeyboardState == STATE_IDLE)
        {
            return(true);
        }

        //
        // Determine how much time has elapsed since we started waiting.  This
        // should be safe across a wrap of g_ui32SysTickCount.
        //
        ui32Now = g_ui32SysTickCount;
        ui32Elapsed = ((ui32Start < ui32Now) ? (ui32Now - ui32Start) :
                     (((uint32_t)0xFFFFFFFF - ui32Start) + ui32Now + 1));
    }

    //
    // If we get here, we timed out so return a bad return code to let the
    // caller know.
    //
    return(false);
}

//*****************************************************************************
//
// Sends a string of characters via the USB HID keyboard interface.
//
//*****************************************************************************
void
SendString(char *pcStr)
{
    uint32_t ui32Char;

    //
    // Loop while there are more characters in the string.
    //
    while(*pcStr)
    {
        //
        // Get the next character from the string.
        //
        ui32Char = *pcStr++;

        //
        // Skip this character if it is a non-printable character.
        //
        if((ui32Char < ' ') || (ui32Char > '~'))
        {
            continue;
        }

        //
        // Convert the character into an index into the keyboard usage code
        // table.
        //
        ui32Char -= ' ';

        //
        // Send the key press message.
        //
        g_eKeyboardState = STATE_SENDING;
        if(USBDHIDKeyboardKeyStateChange((void *)&g_sKeyboardDevice,
                                         g_ppi8KeyUsageCodes[ui32Char][0],
                                         g_ppi8KeyUsageCodes[ui32Char][1],
                                         true) != KEYB_SUCCESS)
        {
            return;
        }

        //
        // Wait until the key press message has been sent.
        //
        if(!WaitForSendIdle(MAX_SEND_DELAY))
        {
            g_bConnected = 0;
            return;
        }

        //
        // Send the key release message.
        //
        g_eKeyboardState = STATE_SENDING;
        if(USBDHIDKeyboardKeyStateChange((void *)&g_sKeyboardDevice,
                                         0, g_ppi8KeyUsageCodes[ui32Char][1],
                                         false) != KEYB_SUCCESS)
        {
            return;
        }

        //
        // Wait until the key release message has been sent.
        //
        if(!WaitForSendIdle(MAX_SEND_DELAY))
        {
            g_bConnected = 0;
            return;
        }
    }
}

//*****************************************************************************
//
// This is the interrupt handler for the SysTick interrupt.  It is used to
// update our local tick count which, in turn, is used to check for transmit
// timeouts.
//
//*****************************************************************************
void
SysTickIntHandler(void)
{
    g_ui32SysTickCount++;
}

//*****************************************************************************
//
// This is the main loop that runs the application.
//
//*****************************************************************************
int
main(void)
{
    uint_fast32_t ui32LastTickCount;
    bool bLastSuspend;


    //
    // Enable lazy stacking for interrupt handlers.  This allows floating-point
    // instructions to be used within interrupt handlers, but at the expense of
    // extra stack usage.
    //
    ROM_FPULazyStackingEnable();

    //
    // Set the clocking to run from the PLL at 50MHz.
    //
    ROM_SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN |
                       SYSCTL_XTAL_16MHZ);

    //
    // Configure the required pins for USB operation.
    //

//    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
//    ROM_GPIOPinConfigure(GPIO_PD2_USB0EPEN);
//    ROM_GPIOPinTypeUSBDigital(GPIO_PORTD_BASE, GPIO_PIN_2);

    // Configure USB0DM & USB0DP (PD4 & PD5)
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
    ROM_GPIOPinTypeUSBAnalog(GPIO_PORTD_BASE, GPIO_PIN_4 | GPIO_PIN_5);

    //Configure USB0ID & USB0VBUS (PB0 & PB1)
//    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
//    ROM_GPIOPinTypeUSBAnalog(GPIO_PORTB_BASE, GPIO_PIN_0 | GPIO_PIN_1);

    //
	// Enable the UART.
	//
	ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
	GPIOPinConfigure(GPIO_PA0_U0RX);
	GPIOPinConfigure(GPIO_PA1_U0TX);
	ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);


	UARTStdioConfig(0, 9600, ROM_SysCtlClockGet());
	UARTprintf("Keyboard device application\n");

    //
    // Erratum workaround for silicon revision A1.  VBUS must have pull-down.
    //
    if(CLASS_IS_TM4C123 && REVISION_IS_A1)
    {
        HWREG(GPIO_PORTB_BASE + GPIO_O_PDR) |= GPIO_PIN_1;
    }

    //
    // Enable the GPIO that is used for the on-board LED.
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
    ROM_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3);
    ROM_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3, 0);

    //
    // Initialize the buttons driver
    //
    ButtonsInit();

    //
    // Not configured initially.
    //
    g_bConnected = false;
    g_bSuspended = false;
    bLastSuspend = false;

    //
    // Initialize the USB stack for device mode.
    //
    //USBStackModeSet(0, eUSBModeDevice, 0);
    USBStackModeSet(0, eUSBModeForceDevice, 0);
    //
    // Pass our device information to the USB HID device class driver,
    // initialize the USB
    // controller and connect the device to the bus.
    //
    USBDHIDKeyboardInit(0, &g_sKeyboardDevice);

    //
    // Set the system tick to fire 100 times per second.
    //
    ROM_SysTickPeriodSet(ROM_SysCtlClockGet() / SYSTICKS_PER_SECOND);
    ROM_SysTickIntEnable();
    ROM_SysTickEnable();

    //
    // The main loop starts here.  We begin by waiting for a host connection
    // then drop into the main keyboard handling section.  If the host
    // disconnects, we return to the top and wait for a new connection.
    //
    while(1)
    {
        uint8_t ui8Buttons;
        uint8_t ui8ButtonsChanged;

        //
        // Tell the user what we are doing and provide some basic instructions.
        //
        UARTprintf("Waiting for host...\n");

        //
        // Wait here until USB device is connected to a host.
        //
        while(!g_bConnected)
        {
        }

        //
        // Update the status.
        //
        UARTprintf("Host connected...\n");

        //
        // Enter the idle state.
        //
        g_eKeyboardState = STATE_IDLE;

        //
        // Assume that the bus is not currently suspended if we have just been
        // configured.
        //
        bLastSuspend = false;

        //
        // Keep transferring characters from the UART to the USB host for as
        // long as we are connected to the host.
        //
        while(g_bConnected)
        {
            //
            // Remember the current time.
            //
            ui32LastTickCount = g_ui32SysTickCount;

            //
            // Has the suspend state changed since last time we checked?
            //
            if(bLastSuspend != g_bSuspended)
            {
                //
                // Yes - the state changed so update the display.
                //
                bLastSuspend = g_bSuspended;
                UARTprintf(bLastSuspend ? "Bus suspended...\n" :"Host connected...\n");
            }

            //
            // See if the button was just pressed.
            //
            ui8Buttons = ButtonsPoll(&ui8ButtonsChanged, 0);
            if(BUTTON_PRESSED(LEFT_BUTTON, ui8Buttons, ui8ButtonsChanged))
            {
                //
                // If the bus is suspended then resume it.  Otherwise, type
                // some "random" characters.
                //
                if(g_bSuspended)
                {
                    USBDHIDKeyboardRemoteWakeupRequest(
                                                   (void *)&g_sKeyboardDevice);
                }
                else
                {
                    SendString("Make the Switch to TI Microcontrollers!");
                }
            }

            //
            // Wait for at least 1 system tick to have gone by before we poll
            // the buttons again.
            //
            while(g_ui32SysTickCount == ui32LastTickCount)
            {

            }
        }

        //
		// Dropping out of the previous loop indicates that the host has
		// disconnected so go back and wait for reconnection.
		//

        if(g_bConnected == false)
        		{
        			UARTprintf("Host disconnected...\n");
        		}

    }
}