Other Parts Discussed in Thread: MAX3232, EK-TM4C123GXL, TM4C123GH6PM
i have done example program of uart echo and i tested port A(A0---->rx,A1---->TX)it's fine,y because the two are internally configured with ICDI. and after that i tested on port B (B0----->rx,B1---->TX)here i configured like this
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
GPIOPinConfigure(GPIO_PB0_U1RX);
GPIOPinConfigure(GPIO_PB1_U1TX);
ROM_GPIOPinTypeUART(GPIO_PORTB_BASE, GPIO_PIN_0 | GPIO_PIN_1);
but here i didn't get any data....to the Terminal......please help me i can i find that?.............thank u