This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ETM Trace configuration macro file (IAR EWB)

Other Parts Discussed in Thread: TM4C129DNCPDT, TM4C129ENCZAD

Does anybody have a macro file that configures the trace pins or the TIVA uCs? FWIW I am using the TM4C129DNCPDT. Debugger is JTAGJet-Trace (Signum).

At the moment I am setting the pins in my application with the function bellow (first thing called by main()).

#define TRACE_PINS (GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | \
                    GPIO_PIN_3 | GPIO_PIN_4)

void
TraceSet(void)
{
    MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
    //
    //First open the lock and select the bits we want to modify in the GPIO commit register.
    //
    HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
    HWREG(GPIO_PORTF_BASE + GPIO_O_CR) = 0x1;

    // Set pins
    MAP_GPIOPinConfigure (GPIO_PF0_TRD2);
    MAP_GPIOPinConfigure (GPIO_PF1_TRD1);
    MAP_GPIOPinConfigure (GPIO_PF2_TRD0);
    MAP_GPIOPinConfigure (GPIO_PF3_TRCLK);
    MAP_GPIOPinConfigure (GPIO_PF4_TRD3);

    MAP_GPIODirModeSet(GPIO_PORTF_BASE, TRACE_PINS, GPIO_DIR_MODE_HW);
    MAP_GPIOPadConfigSet(GPIO_PORTF_BASE, TRACE_PINS, GPIO_STRENGTH_2MA,
                     GPIO_PIN_TYPE_STD);
}

Trace clock and data lines show activity. However I am getting some weird behaviour from C-Spy (a lot of garbage along with some data that makes sense. Perhaps C-Spy expects the trace lines to be functional when the debugging session starts. IAR documentation says one should create a macro file to do so. They mention some examples (ETM_init*.mac) for some processors but none for TI's.

I would like to try the configuration with a macro file instead of in the application so I would appreciate if somebody that crafted such a macro file could share it. I may try to craft it myself based on one of the examples I found but I had rather skip what may be a time consuming endeavor if I can.

Thank you in advance for any help.