Other Parts Discussed in Thread: ENERGIA
I have hardware PWM working but I can't get it to appear on any pins other than the three that drive the LEDs. Is my code wrong?
In this case I'm looking for a PWM signal on PF0 and PA6 but not finding it.
/*################################################
# Hardware PWM proof of concept using
# the Tiva C Launchpad
#
# Started with example code by
# lawrence_jeff found here:
# http://forum.stellarisiti.com/topic/707-using-hardware-pwm-on-tiva-launchpad/
#
# Altered to use code found on section
# 22.3 of the TivaWare Peripheral Driver
# Library User's Guide found here:
# http://www.ti.com/lit/ug/spmu298a/spmu298a.pdf
#
#
# This example pulses three on-board LEDs
#
#################################################*/
#include "driverlib/pin_map.h"
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_gpio.h"
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "driverlib/sysctl.h"
#include "driverlib/pin_map.h"
#include "driverlib/gpio.h"
#include "driverlib/pwm.h"
void delayMS(int ms) {
SysCtlDelay( (SysCtlClockGet()/(3*1000))*ms ) ;
}
int main(void)
{
//Set the clock
SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
//Configure PWM Clock to match system
SysCtlPWMClockSet(SYSCTL_PWMDIV_64);
// Enable the peripherals used by this program.
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM1); //The Tiva Launchpad has two modules (0 and 1). Module 1 covers the LED pins
//Configure PF1,PF2,PF3 Pins as PWM
GPIOPinConfigure(GPIO_PA6_M1PWM2);
GPIOPinConfigure(GPIO_PF0_M1PWM4);
GPIOPinConfigure(GPIO_PF1_M1PWM5);
GPIOPinConfigure(GPIO_PF2_M1PWM6);
GPIOPinConfigure(GPIO_PF3_M1PWM7);
GPIOPinTypePWM(GPIO_PORTA_BASE, GPIO_PIN_6);
GPIOPinTypePWM(GPIO_PORTF_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3);
//Configure PWM Options
//PWM_GEN_2 Covers M1PWM4 and M1PWM5
//PWM_GEN_3 Covers M1PWM6 and M1PWM7 See page 207 4/11/13 DriverLib doc
PWMGenConfigure(PWM1_BASE, PWM_GEN_1, PWM_GEN_MODE_DOWN | PWM_GEN_MODE_NO_SYNC);
PWMGenConfigure(PWM1_BASE, PWM_GEN_2, PWM_GEN_MODE_DOWN | PWM_GEN_MODE_NO_SYNC);
PWMGenConfigure(PWM1_BASE, PWM_GEN_3, PWM_GEN_MODE_DOWN | PWM_GEN_MODE_NO_SYNC);
unsigned long period = 5000;
unsigned long pwmNow = period/10;
//Set the Period (expressed in clock ticks)
PWMGenPeriodSet(PWM1_BASE, PWM_GEN_1, period);
PWMGenPeriodSet(PWM1_BASE, PWM_GEN_2, period);
PWMGenPeriodSet(PWM1_BASE, PWM_GEN_3, period);
//Set PWM duty-50% (Period /2)
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_1,pwmNow);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_4,pwmNow); //90 degrees
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_5,pwmNow); //90 degrees
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_6,pwmNow);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_7,pwmNow);
// Enable the PWM generator
PWMGenEnable(PWM1_BASE, PWM_GEN_1);
PWMGenEnable(PWM1_BASE, PWM_GEN_2);
PWMGenEnable(PWM1_BASE, PWM_GEN_3);
// Turn on the Output pins
PWMOutputState(PWM1_BASE, PWM_OUT_2_BIT | PWM_OUT_4_BIT | PWM_OUT_5_BIT | PWM_OUT_6_BIT | PWM_OUT_7_BIT, true);
//Fade
bool fadeUp = true;
unsigned long increment = 10;
while(1)
{
/*
delayMS(2000);
pwmNow = period/20;
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_4,pwmNow);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_5,pwmNow);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_6,pwmNow);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_7,pwmNow);
delayMS(2000);
pwmNow = period/10;
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_4,pwmNow);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_5,pwmNow);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_6,pwmNow);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_7,pwmNow);
*/
}
}