hello friends
i have installed ccs 5.5.0. when i debug any project then debugger automatically start running. actually it should wait for pressing of Run button before running. also program is not halting at breakpoints. Any suggestion?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello friends
i have installed ccs 5.5.0. when i debug any project then debugger automatically start running. actually it should wait for pressing of Run button before running. also program is not halting at breakpoints. Any suggestion?
Hello Sanjay,
What is the debugger that you are using and which Tiva Processor is that you are using. Also it would be worthwhile to share the ccxml file and/or CCS project.
Regards
Amit
Hi amit
i'm using stellaris In-circuit debuuger(ICDI) with tiva c series tm4c1294xl as controller.
One more thing is that same project is running well on another system.
thanks
Er. Sanjay
Hello Sanjay,
Can you share the console log from CCS? Also the information is too sketchy to get any real problem isolated. Is this a connected LaunchPad or are you using the Stellaris-ICDI wired to a custom board?
Regards
Amit
Hello Amit
Actually i installed ccs in another system and that is working fine.
so i think my earlier system is having some issue.
By the thanks a lot for the support.
Er. Sanjay
Hello Sanjay,
Could be. Can you uninstall CCS and re-install the same. It's always good to have multiple systems...
Regards
Amit