Other Parts Discussed in Thread: TM4C1290NCZAD
Hi,
In a new design I want to use the TM4C1290NCZAD. Since the application is a low power application, most of the environmetn is working at 1.8V, thus except of the VDD 3.3V to the TM4C129 all the rest are supplied with 1.8V (UARTs, GPIOs, I2C, SPIs, etc.)
Can the TM4C129 work in this kind of an environment?
Doe's the GPIOs support 1.8V inputs?
What about the UARTs?