We want to store key data in the battery backed RAM in the TM4C129ENCPDTI3's hibernate module. Does this memory have a finite number of writes similar to Flash memory, or is it like RAM where there is an infinite number of writes?
Thanks,
Bill
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We want to store key data in the battery backed RAM in the TM4C129ENCPDTI3's hibernate module. Does this memory have a finite number of writes similar to Flash memory, or is it like RAM where there is an infinite number of writes?
Thanks,
Bill
Bill Sousan said:...is it like RAM where there is an infinite number of writes?
In general agree w/poster Roberto - yet does not this detail reside w/in MCU manual - buried deep in the cheap seats? (MCU electrical specs - usually organized/grouped by MCU peripheral - found at the very end of the manual)
Expect to see voltage minimums, current requirements, and (one hopes) any such usage restrictions/limitations/life issues...
Final point - modern MCUs have vastly expanded number of Flash writes - unless your application is, "machine gunning" such "key data" during "live" operation - it seems Flash will provide an acceptable alternative.
Hello All
My 2 cents on the topic: The Key data if critical must not be stored on something accessible like the Battery backed RAM, but on the EEPROM which can be secured using Password.
Other than that Roberto and cb1, thanks.
Regards
Amit
What if that "key data" is to be, "Quickly Saved?" Would use of the "password" and access time penalties incurred by EEPROM prove ideal?
The use and activity of such "key data" may dictate poster's "best handling" of such "key data." A "universal approach" may not satisfy all masters...
Hello cb1
Yes, indeed if it needs to be quickly saved, then BBRAM is a good place, but then the "key" is very loosely defined as well. Is this some encryption/decryption key or a important variable value to be used key.
Regards
Amit
Yes in my case it needs to be quickly saved and saved often (and is only 32 bytes long). "Key" data refers to data that needs to be saved - but not encrypted/secure. So for my app, I think the battery backed RAM makes sense.
Thanks for your insight,
Best,
Bill
Thanks to cb1 for bringing up the topic as well with a well considered view
Regards
Amit
Thanks for that kind mention, Amit.
Many years in the MCU, FPGA, & memory trenches leads to a, "bigger picture" view. It's (often) necessary to tease out poster's real application - even when that may reduce or eliminate the full recitation (and use) of all MCU features.
Indeed the MCU's EEPROM adds value - yet the whole of the application must always be fully/properly considered - only then is the best/most appropriate MCU feature-handling revealed.