Other Parts Discussed in Thread: TMS570LS3137
Hi,
We are using TMS570LS3137 processor in custom board and using 20MHz oscillator for clkin input. In two boards (some boards are working fine), we are facing oscillator failure status flag issue. But the oscillator is at 20MHz and don't see any issue. So we programmed the ECLK output to OSC option and measured frequency is 4.79MHz frequency and oscillator fail status bit is also set. I would like to know why we are getting 4.79MHz instead of 20MHz in ECLK output and also why the oscillator fail flag bit is set when the oscillator is within the range? How to resolve this issue?
regards