Other Parts Discussed in Thread: TMS570LC4357, RM57L843, TPS54350
Hello,
I have gone through the discussions related PMU for TMS570LC4357, but couldn't conclude my self.
I am looking for PMU for TMS570LC4357. I am going to inteface 4 CAN transceivers with this controller. No other interfaces used.
My input Voltage: 5 V to 15V.
Outputs:
1 . 3.3V for CAN transcevers (280 mA Max) and Digital logic supply voltage (I/O) & Flash pump supply voltage of controller.
2. 1.2V for Digital logic supply voltage (Core)
Kindly suggest PMU with monotoring and saftey crital features. And i have TMS570LC43x Hercules Development Kit. But i couldn't find schematics for the same. How to get the schematcs ??
Thanks in advance.
Regards,
Govind.