This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FreeRTOS+Trace code error

Other Parts Discussed in Thread: HALCOGEN, TMS570LS0432

I use Hercules Launchpad TMS570LS0432 kit and FreeRTOS v8.1.2, and I use Halcogen for code generation. I tried inserting code for Trace Options available with Tracealyzer from Percepio(FreeRTOS+Trace). After adding the necessary header and source file provided by percepio into the project, code build results in error

 error #10099-D: program will not fit into available memory.  run placement with alignment fails for section ".kernelHEAP" size 0x2800 .  Available memory ranges:
   RAM          size: 0x6300       unused: 0x1a50       max hole: 0x1a50   

The software uses on chip RAM for recording the Trace. Kindly suggest a solution to get rid of this error