Other Parts Discussed in Thread: TMS570LC4357
Dear all,
I would like to discuss a way how to connect the latest Hercules microcontroller TMS570LC4357 in the SPI parallel mode with NOR flash Micron N25Q00AA operating in the Quad mode/protocol.
If I understood correctly, there is a fundamental obstacle to connect the micro with the flash:
TMS570LC4357 supports the 4-datachannel SPI5 (transferring 16bit word) - signals SIMO[0..3] and SOMI [0..3]. But the memory N25Q00AA uses signals DQ0 - DQ3 as bi-directional I/O pins.
Do you have any idea how to configure and establish the connection between those two devices? In the HW point of view as well as within the SPI peripheral setting?
Many thanks in advance,
Best regards, Jiri
.