Other Parts Discussed in Thread: UNIFLASH, HALCOGEN
Hi there!
I'm trying to flash a TMS570 DK but suddenly, the flashing do not works how it should... I tryed to find some solution, but I only found out discontinued discutions...
Actually I tried with more than one tools to flash. The answers are:
CCS UniFlash:
[17:09:18] Start operations on multiple programs on the target core...
[17:09:18] Loading program: C:\workspace\W5\p2\Debug\p2.out
[17:09:18] WARNING >> CortexR4: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
[17:09:24] ERROR >> CortexR4: File Loader: Data verification failed at address 0x00000000 Please verify target memory and memory map.
[17:09:24] ERROR >> CortexR4: GEL: File: C:\workspace\W5\p2\Debug\p2.out: a data verification error occurred, file load failed.
[17:09:25] File: C:\workspace\W5\p2\Debug\p2.out: a data verification error occurred, file load failed.
[17:09:25] Programs operation finished.
CCSv5.5.0:
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0CortexR4: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
I only want to mention that until today all worked fine.
I also added the *.gel files and the sys_link.cmd file. I saw that is useful... :)
I would like to specify that in CSS (v4, v5, v6) on the flashing tab (in Debug) I have no AutomaticECC nor something else...
Thanks in advance. Mihai.