Hi,
I need to drive an H-Bridge circuit with Tiva C Series TM4C123G LaunchPad at frequencies starting from 10 Hz to 200 Hz. I tried to use deadband property of PWM modules however it does not work at 100 Hz. I couldn't generate 10 Hz PWM. I don't want to write any code with polling method because I have other stuff to do at the same time such as UART connection with PC. Is there any way to generate such signals.
Thanks for your help.
huseyin