Other Parts Discussed in Thread: TM4C1294NCPDT
Hi there,
I am going to write a driver for an AD5754 digital analog converter class. I am not able to dynamically create an object with the new operator. In an other thread I read that the heap size is zero on an other board. But I can not find the tcf file to configure the heap size manually. I have a file named "tm4c1294ncpdt.cmd" which says this in a comment:
/* The following command line options are set as part of the CCS project. */ /* If you are building using the command line, or for some reason want to */ /* define them here, you can uncomment and modify these lines as needed. */ /* If you are using CCS for building, it is probably better to make any such */ /* modifications in your CCS project and leave this file alone. */ /* */ /* --heap_size=0 */ /* --stack_size=256 */ /* --library=rtsv7M4_T_le_eabi.lib */
Where do I have to write --heap_size=65536 or similar?
Thank you!