Other Parts Discussed in Thread: TM4C1233H6PZ, UNIFLASH, LMFLASHPROGRAMMER
Hello Tiva C Series Team,
I am working with a custom board with the TM4C1233H6PZ. Until last week the processor was running without any issue in our labs and testbeds on several boards. At beginning this week we shipped two boards to a different location and after a operation time of about an hour respectively 3 days the TM4C1233H6PZ died. This means there is no code execution of the processor. By now investigations had the results:
- External supply voltage: OK
- Voltage of internal LDO at VDDC: OK
- No signal at OSCOUT; the application uses a external crystal
- No connection to debug port possible
- Hibernation module not used; wake pin pulled to low
- The case is heated up to about 43°C
Since the case temperature is about 43°C it seams to me, that the processor core is still working, but without any reaction the the surrounding.
Has anybody an idea on further investigations or to reanimate the TM4C1233H6PZ?
Thanks in advance
Thomas