This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART Interrupt error

#20 identifier "INT_UART0_" is undefined main.c /test_erode line 53 C/C++ Problem

please suggest the change in the code given below.

------------------------------------

#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"


#define GPIO_PA0_U0RX 0x00000001

#define GPIO_PA1_U0TX 0x00000401


void UARTIntHandler(void)
{
uint32_t ui32Status;

ui32Status = UARTIntStatus(UART0_BASE, true); //get interrupt status

UARTIntClear(UART0_BASE, ui32Status); //clear the asserted interrupts

while(UARTCharsAvail(UART0_BASE)) //loop while there are chars
{
UARTCharPutNonBlocking(UART0_BASE, UARTCharGetNonBlocking(UART0_BASE)); //echo character
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, GPIO_PIN_2); //blink LED
SysCtlDelay(SysCtlClockGet() / (1000 * 3)); //delay ~1 msec
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0); //turn off LED
}
}

int main(void) {

SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);

SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);

SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF); //enable GPIO port for LED
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_2); //enable pin for LED PF2

UARTConfigSetExpClk(UART0_BASE, SysCtlClockGet(), 115200,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));

IntMasterEnable(); //enable processor interrupts
IntEnable(INT_UART0); //enable the UART interrupt
UARTIntEnable(UART0_BASE, UART_INT_RX | UART_INT_RT); //only enable RX and TX interrupts

UARTCharPut(UART0_BASE, 'E');
UARTCharPut(UART0_BASE, 'n');
UARTCharPut(UART0_BASE, 't');
UARTCharPut(UART0_BASE, 'e');
UARTCharPut(UART0_BASE, 'r');
UARTCharPut(UART0_BASE, ' ');
UARTCharPut(UART0_BASE, 'T');
UARTCharPut(UART0_BASE, 'e');
UARTCharPut(UART0_BASE, 'x');
UARTCharPut(UART0_BASE, 't');
UARTCharPut(UART0_BASE, ':');
UARTCharPut(UART0_BASE, ' ');

while (1) //let interrupt handler do the UART echo function
{
// if (UARTCharsAvail(UART0_BASE)) UARTCharPut(UART0_BASE, UARTCharGet(UART0_BASE));
}

}